2017-02-15 6:11 AM
Posted on February 15, 2017 at 15:11
I've not been able to get the Audio Recorder in the demonstration software working. I'm using V1.2 of the software, as supplied with Cube V1.6.0.
Test:
When I do this, the red button goes blue and the software hangs (including the UI and the USB driver) until the board is rebooted.
I've tried debugging the recorder and found that:
Ideas on any or all of the following would be most welcome:
Cheers,
JB.
Solved! Go to Solution.
2017-02-15 6:14 PM
Posted on February 16, 2017 at 02:14
I've solved the problem. It was indeed because DMA 2 stream 4 did not have an interrupt handler. This was due to a combination of:
The Cube bug is in lines 191 to 193 of the above file. These lines specify DMA2_Stream0 but should instead specify DMA2_Stream4.
♯define AUDIO_DFSDMx_DMAx_TOP_LEFT_STREAM DMA2_Stream0 /* JSB: Should be DMA2_Stream4 */
♯define AUDIO_DFSDMx_DMAx_TOP_LEFT_IRQ DMA2_Stream0_IRQn /* JSB: Should be DMA2_Stream4_IRQn */
♯define AUDIO_DFSDMx_DMAx_TOP_LEFT_IRQHandler DMA2_Stream0_IRQHandler
/* JSB: Should be DMA2_Stream4_IRQHandler*/
The result is consistent with the following three blocks of code (and works).
The Eclipse build issue was an odd one:
There are two versions of both stm32f769i_discovery_audio.h and stm32f769i_discovery_audio.c: one in the project and the other in '<Cube>/Drivers/BSP/STM32F769I-Discovery'.
Crucially, the version of stm32f769i_discovery_audio.h in the project does not have the above bug.
Somehow Eclipse was compiling stm32f769i_discovery_audio.c in the project with stm32f769i_discovery_audio.h in the project, but stm32f7xx_it.c in the project with stm32f769i_discovery_audio.h in '<Cube>/Drivers/BSP/STM32F769I-Discovery'.
As a result, stm32f769i_discovery_audio.c was producing DMA 2 stream 4 interrupts but stm32f7xx_it.c was handling DMA 2 stream 0 interrupts. DMA 2 Stream 4 interrupts were therefore not handled, resulting in the audio recorder hanging, which was the original problem.
Incidentally, if '<Cube>/Drivers/BSP/STM32F769I-Discovery/stm32f769i_discovery_audio.h' is used throughout, i.e. by both stm32f769i_discovery_audio.c and stm32f7xx_it.c, e.g. by renaming the version in the project to force the compiler to look further, then the Audio Recorder works again, despite the above header file bug. This is because DMA 2 stream 0 interrupts are then both produced and handled, even though they should be stream 4 ones. Nevertheless, that's not a good reason to stick with the bug, for obvious reasons. Therefore, it would be helpful for the bug to be fixed.
JB.
2017-02-15 9:50 AM
Hello,
Did you tried the ready example in the STM32CubeF7 firmware package and follow the instructions on the readme files?
STM32Cube_FW_F7_V1.6.0\Projects\STM32F769I-Discovery\Applications\Audio\Audio_playback_and_record
I suggest you to debug, localize where the code hangs and precise what do you have exactly as an error message.
You may refer to this describing how to use the audio recording application, it maybe helpful.Hope this helps you.
Regards
Imen
2017-02-15 11:23 AM
Posted on February 15, 2017 at 19:23
Hi Imen.
I've previously tried compiling the Audio_playback_and_record standalone example and that works fine. However, I've not yet managed to learn anything from it that has helped with fixing the Demostration Software audio recorder.
I've studied AN3997, which incidently is for the F4 Discovery rather than F7, but it is not at an appropriate level of detail for the problem in hand.
I've cut the demonstration software down to just the audio recorder (to greatly reduce the built and programming time).
Then, by using the Default_Handler in http://www.freertos.org/Debugging-Hard-Faults-On-Cortex-M-Microcontrollers.html, I've found that DMA 2 stream 4 does not have an interrupt handler. I'm currently looking into why this is.
JB.
2017-02-15 6:14 PM
Posted on February 16, 2017 at 02:14
I've solved the problem. It was indeed because DMA 2 stream 4 did not have an interrupt handler. This was due to a combination of:
The Cube bug is in lines 191 to 193 of the above file. These lines specify DMA2_Stream0 but should instead specify DMA2_Stream4.
♯define AUDIO_DFSDMx_DMAx_TOP_LEFT_STREAM DMA2_Stream0 /* JSB: Should be DMA2_Stream4 */
♯define AUDIO_DFSDMx_DMAx_TOP_LEFT_IRQ DMA2_Stream0_IRQn /* JSB: Should be DMA2_Stream4_IRQn */
♯define AUDIO_DFSDMx_DMAx_TOP_LEFT_IRQHandler DMA2_Stream0_IRQHandler
/* JSB: Should be DMA2_Stream4_IRQHandler*/
The result is consistent with the following three blocks of code (and works).
The Eclipse build issue was an odd one:
There are two versions of both stm32f769i_discovery_audio.h and stm32f769i_discovery_audio.c: one in the project and the other in '<Cube>/Drivers/BSP/STM32F769I-Discovery'.
Crucially, the version of stm32f769i_discovery_audio.h in the project does not have the above bug.
Somehow Eclipse was compiling stm32f769i_discovery_audio.c in the project with stm32f769i_discovery_audio.h in the project, but stm32f7xx_it.c in the project with stm32f769i_discovery_audio.h in '<Cube>/Drivers/BSP/STM32F769I-Discovery'.
As a result, stm32f769i_discovery_audio.c was producing DMA 2 stream 4 interrupts but stm32f7xx_it.c was handling DMA 2 stream 0 interrupts. DMA 2 Stream 4 interrupts were therefore not handled, resulting in the audio recorder hanging, which was the original problem.
Incidentally, if '<Cube>/Drivers/BSP/STM32F769I-Discovery/stm32f769i_discovery_audio.h' is used throughout, i.e. by both stm32f769i_discovery_audio.c and stm32f7xx_it.c, e.g. by renaming the version in the project to force the compiler to look further, then the Audio Recorder works again, despite the above header file bug. This is because DMA 2 stream 0 interrupts are then both produced and handled, even though they should be stream 4 ones. Nevertheless, that's not a good reason to stick with the bug, for obvious reasons. Therefore, it would be helpful for the bug to be fixed.
JB.
2017-02-16 5:05 AM
Hello
Bladen.John
,Thanks for sharing your solution and feedback.
I will report internallythis issuefor checking and working andI will come back to you as soon as I have needed details.
Imen
2017-02-16 7:14 AM
Posted on February 16, 2017 at 15:14
Thanks Imen.
In addition:
♯define AUDIO_DFSDMx_DMAx_LEFT_IRQ DMA2_Stream0_IRQn
♯define AUDIO_DFSDMx_DMAx_RIGHT_IRQ DMA2_Stream5_IRQn
♯define AUDIO_DFSDM_DMAx_LEFT_IRQHandler DMA2_Stream0_IRQHandler
♯define AUDIO_DFSDM_DMAx_RIGHT_IRQHandler DMA2_Stream5_IRQHandlershould be:
♯define AUDIO_DFSDMx_DMAx_LEFT_IRQ DMA2_Stream4_IRQn
♯define AUDIO_DFSDMx_DMAx_RIGHT_IRQ DMA2_Stream5_IRQn
♯define AUDIO_DFSDM_DMAx_LEFT_IRQHandler DMA2_Stream4_IRQHandler
♯define AUDIO_DFSDM_DMAx_RIGHT_IRQHandler DMA2_Stream5_IRQHandlerin file '<,STM32Cube_FW_F7_V1.6.0\Drivers\BSP\STM32F769I_EVAL\stm32f769i_eval_audio.h'.
Please pass this on too.
Cheers,
JB.
2017-02-16 8:56 AM
Posted on February 16, 2017 at 16:56
And there's a possible error here too, again in 'STM32Cube_FW_F7_V1.6.0\Drivers\BSP\STM32F769I-Discovery\stm32f769i_discovery_audio.h':
♯define AUDIO_DFSDMx_TOP_RIGHT_CHANNEL DFSDM_CHANNEL_0
♯define AUDIO_DFSDMx_TOP_LEFT_CHANNEL DFSDM_CHANNEL_1
♯define AUDIO_DFSDMx_BUTTOM_RIGHT_CHANNEL DFSDM_CHANNEL_4
♯define AUDIO_DFSDMx_BUTTOM_LEFT_CHANNEL DFSDM_CHANNEL_5This should possibly be:
♯define AUDIO_DFSDMx_TOP_LEFT_CHANNEL DFSDM_CHANNEL_0
♯define AUDIO_DFSDMx_TOP_RIGHT_CHANNEL DFSDM_CHANNEL_1
♯define AUDIO_DFSDMx_BOTTOM_LEFT_CHANNEL DFSDM_CHANNEL_4
♯define AUDIO_DFSDMx_BOTTOM_RIGHT_CHANNEL DFSDM_CHANNEL_5For consistency with Cube code elsewhere. This involves swapping channels 0 and 1, and swapping channels 4 and 5. I've not checked whether this is correct with the F769 Discovery board. FWIW, on the schematic the two top sensors connect to DFSDM_DATIN1, and the two bottom sensors connect to DFSDM_DATIN5. I've not investigated how these signals are used in the MCU.
Please pass this on too.
Cheers,
JB.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.