STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Custom external bootloader on custom F769I based Board

Posted on March 16, 2017 at 18:29Hi community,I need to write an external bootloader for my custom board based on the stm32f769I MCU.According to the 'STM32 ST-LINK utility software description' manual, I have to modify one of the exemple provided a...

enia ami by Associate II
  • 2977 Views
  • 6 replies
  • 0 kudos

Audio_Sampling_frequency

Posted on March 17, 2017 at 10:30Hi all,I am working on memsmic1 application which is convert 1 bit pdm data into pcm. with sampling frequency 16 Khzif#define AUDIO_CHANNELS 2#define AUDIO_SAMPLING_FREQUENCY 16000 #if (AUDIO_SAMPLING_FREQUENCY == 16...

How to revive a dead MCU in-circuit?

Posted on December 18, 2016 at 15:11Hello all!  How's this for my very first question I purchased a 3d Printer on clearance with a tag that says Does not Start up.  No warranty.  I was ok with that.  As I'm a developer and a hardware hacker I knew I...

Resolved! STM32F437 timer input capture

Posted on March 16, 2017 at 20:16I have attempted to set up timer 4 channel 1 for input capture but unsuccessfully. The scope indicates that my 1KHz, 3vdc, 35 uSec pulses are making it to PD12 (TIM4, ch 1). However, CC1IF is never set. Although chan...

John Hite by Associate III
  • 1915 Views
  • 5 replies
  • 0 kudos

Character match interrupt

Posted on March 17, 2017 at 13:29Hello,       I'm going to use the 'Character match interrupt' to identify the end (\n) of the message received from an USART. (on an STM32L4 Series ).Since I am quite new to this world, I did various tests, but I cou...

I think LDO Power is lack on STM32F746-DISCO Board.

Posted on March 17, 2017 at 02:07I test audio recorder/player on STM32F746-DISCO board.So, WM8944(codec) drive speaker(2W) out.But, TFT-LCD was break sometimes at full volume level.So, I think LDO Power is lack on STM32F746-DISCO board.

I want to adjust duty cycle.

Posted on March 17, 2017 at 07:39I used TIM1_channel 1  and channel 3 .TIM3 use ADC triigger.so I want to update TIM1 duty cylce.I wrote code below.HAL_TIM_PWM_Start(&htim1,TIM_CHANNEL_1); __HAL_TIM_SET_COMPARE(&htim1,TIM_CHANNEL_1,detact_pulse);HAL...

i want to use ADC with trigger mode

Posted on March 16, 2017 at 02:05I have used stm32f303vdt with cubemxbut i updated cubemx ver.4.19i want to use ADC with trigger mode ADC1 have trigger mode  but ADC2 don/'t have triggermodehow can i solve it?(before i used ADC1,2 trigger mode but W...

0690X00000606ZbQAI.png 0690X00000606ZkQAI.png

How to interface Dual Digital Mic with Stm32f407 ?

Posted on March 17, 2017 at 07:44Hello everyone,I am using stm32f4 discovery board. i am accessing on board digital mic with I2S protocol and decode data using PDM to PCM library from st.Now i want to use one more mic for stereo audio (one mic for l...

STM32f429 TIM9 PWM setup

Posted on March 17, 2017 at 02:58I am sure this has been asked 1000 times, but I still cannot get the results I need.  I am trying to generate a 12800000 clock output on TIM9 with a 50% duty cycle.  I have looked at the code examples.  I have the AP...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.