2017-03-16 12:16 PM
I have attempted to set up timer 4 channel 1 for input capture but unsuccessfully. The scope indicates that my 1KHz, 3vdc, 35 uSec pulses are making it to PD12 (TIM4, ch 1). However, CC1IF is never set. Although channels 2-4 are not configured CC2IF - CC4IF are being set and thus so is UIF but my ISR is never called. So I have two problems no CC1IF and no call to the ISR. Suggestions and advice would be much appreciated. The code follows.
Thanks,
JH
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
uint32_t rpm4;
void RpmTask(void *p_arg);void RpmTask(void *p_arg)
{ static int i = 0; uint16_t itstatus = 0;GPIO_StructInit(&GPIO_InitStruct);
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_12; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStruct.GPIO_Speed = GPIO_High_Speed; GPIO_Init(GPIOD, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOD, GPIO_PinSource12, GPIO_AF_TIM4);NVIC_InitTypeDef NVIC_InitStruct;
NVIC_InitStruct.NVIC_IRQChannel = TIM4_IRQn; NVIC_InitStruct.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStruct.NVIC_IRQChannelSubPriority = 0; NVIC_InitStruct.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStruct);//RPM timer setups
// APB1PeriphClock - 42 MHz // APB2PeriphClock - 84 MHz RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3 | RCC_APB1Periph_TIM4, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 | RCC_APB2Periph_TIM9, ENABLE);TIM_TimeBaseInitTypeDef tim4_base;
tim4_base.TIM_Period = 0xFFFFFFFF; tim4_base.TIM_Prescaler = 48; tim4_base.TIM_ClockDivision = TIM_CKD_DIV1; //digital filter clk div, don't care, filtering is off tim4_base.TIM_CounterMode = TIM_CounterMode_Up; tim4_base.TIM_RepetitionCounter = 0; //t1&t8 pwm, don't care TIM_TimeBaseInit(TIM4, &tim4_base);TIM_ICInitTypeDef tim4_icInit;
tim4_icInit.TIM_Channel = TIM_Channel_1; tim4_icInit.TIM_ICPolarity = TIM_ICPolarity_Rising; //r, f, both tim4_icInit.TIM_ICSelection = TIM_ICSelection_DirectTI; //dir, ind, trc tim4_icInit.TIM_ICPrescaler = TIM_ICPSC_DIV1; //1-8 tim4_icInit.TIM_ICFilter = 0x0; TIM_ICInit(TIM4, &tim4_icInit);/* Enable the CC2 Interrupt Request */
TIM_ITConfig(TIM4, TIM_IT_CC1, ENABLE);/* TIM enable counter */
TIM_Cmd(TIM4, ENABLE);while (1)
{ rpm4 = TIM_GetCounter(TIM4); itstatus = TIM4->SR; }}void timer4_isr(void)
{ if (TIM_GetITStatus(TIM4, TIM_IT_CC1) == SET) { TIM_ClearITPendingBit(TIM4, TIM_IT_CC1); rpm4 = TIM_GetCounter(TIM4); }TIM_ClearITPendingBit(TIM4, TIM_IT_Update);
}#input-captureSolved! Go to Solution.
2017-03-16 4:37 PM
Timer registers look all OK (FYI checked in this order: CCMR1.CC1S if set to 'straight in'; CCER.CC1E if set to enable; DIER.CC1IE if set to enable).
Went to the GPIO registers, this was the very first to check:
MODER 0x5455555A
Lower two bits of that nibble are 00 which means that MODE of pin 12 is *not* AF as it is supposed to be, but In.
Now going in reverse:
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_IN;
I don't 'library' but this is probabaly the culprit.
JW
2017-03-16 12:48 PM
Post the content of relevant GPIO and TIM registers.
Did you observe the input signal directly on the MCU pin?
JW
2017-03-16 2:35 PM
First perhaps I should have stated that I am trying to measure RPM counting the time between pulses.
Yes I piled on two pair of reading glasses and put my scope probe right on pin 81 of the 144 pin package.
I will collect the registers now. The TIM4 registers are below. Which GPIO registers would be useful?
cr1 0x0001
cr2 0x0000 dier 0x0002 sr 0x001D egr 0x0000 ccmr1 0x0001 ccmr2 0x0000 ccer 0x0001 psc 0x0064 arr 0xFFFF ccr1 0x0000 ccr2 0x00002017-03-16 3:07 PM
Figured out how to get the watch list to give me GPIOD...
gpiod 0x40020C00
MODER 0x5455555AOTYPER 0x00000000OSPEEDR 0x0000000FPUPDR 0x00000000IDR 0x0000000BODR 0x00000008BSRRL 0x0000 BSRRH 0x0000 LCKR 0x00000000AFR <array> [0] 0x00000099 [1] 0x000200002017-03-16 4:37 PM
Timer registers look all OK (FYI checked in this order: CCMR1.CC1S if set to 'straight in'; CCER.CC1E if set to enable; DIER.CC1IE if set to enable).
Went to the GPIO registers, this was the very first to check:
MODER 0x5455555A
Lower two bits of that nibble are 00 which means that MODE of pin 12 is *not* AF as it is supposed to be, but In.
Now going in reverse:
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_IN;
I don't 'library' but this is probabaly the culprit.
JW
2017-03-17 6:40 AM
JW,
Yes, that was it! Thank you very much for taking the time to look through all my register settings, I know that took some time.
I inherited the GPIO from a 'working' sister project and I assumed that all of the GPIO settings were correct as they have been until now. This is my mistake, I blame no one but myself for failing to see this.
Thank you again,
JH
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.