STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DCMI to memory, memory to UART, DMA Transfer

Posted on September 25, 2013 at 13:01Hi,I want to receive datas from DCMI interface and then transfer it to UART interface through DMA.To do that, I am plannig to receive each Byte from the DCMI interface store it into a buffer using DMA and then tr...

1 uS delay with timer ?

Posted on March 19, 2017 at 21:51Hello Everyone,Does every one know on how to create a simple 1 uS delay with timer ?Thanks#stm32f1xx #timer #delay-1us

Calculate rcc with stm32f10x

Posted on March 14, 2017 at 17:23Hi,Here is my input datayou assume that I have 4 variables such as Data1,Data2,Data3 and Data4 that store each byte (Data1 saves d24-d31 and Data4 stores D0-D7). So I want to know how can I execute Crc-8 algorithm in...

0690X00000606F3QAI.png
parisa by Senior
  • 2655 Views
  • 9 replies
  • 0 kudos

''ARM compiler for MCU'' ver. 1.13.2 Error in System Workbench

Posted on March 18, 2017 at 10:48Hi,Recently I upgrade the 'ARM compiler for MCU' in System Workbench to 1.13.2 after which I am getting the following error as displayed in the console :/usr/make/sh: arm-none-eabi-gcc: command not foundmake: *** [Da...

RADS1 by Associate II
  • 736 Views
  • 0 replies
  • 0 kudos

STM32L053 EEPROM writing going to HardFault

Posted on March 17, 2017 at 23:00Hi!I am trying to write s string into the EEPROM of a STM32L053.I create a strcpy like funtion, using STM32L0xx HAL Libraries:for writing the EEPROM I use this sequence of HAL functions.char ascii_string[200];HAL_FLA...

CAN Initialization on extremely high traffic

Posted on March 17, 2017 at 21:30Hi, my software stucks on CAN_MSR_INAK acknowledge when I try to init CAN in device that is connected to network with very high traffic. From reference manual I've found that:  Once 11 consecutive recessive bits have...

SMTF32F1x CAN bus Error Frame

Posted on February 17, 2017 at 18:54Hi,I am seeing Error Frame from one of our project using STM32F1x MCU. Any recommendation how to debug this issue?Thanks,Dick112.227000 1 108 Rx d 8 db 1f c0 69 ee 89 e8 3e 112.227000 1 109 Rx d 8 86 31 94 43 00 ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.