STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32N6 boot from eMMC

1. Setup OTPThe default OTP configuration of the chip is to boot from norflash, so you need to modify OTP to boot from EMMC. (Note: OTP can only be modified once, please operate with caution!)Open STM32CubeProgrammer software, check OTP_FUSES_STM32N6...

640.png 640 (1).png 640 (2).png 640 (3).png

Resolved! How to wake up from standby mode?

I am using an stm32c011 MCU and want to put my device into standby mode and then periodically wake it up (every 30s or so).I have seen guides which use the RTC to do that, but cube mx doesn't show me a WakeUp option on my RTCAm I missing something or...

DavidL__0-1738849020205.png
DavidL_ by Associate III
  • 3979 Views
  • 9 replies
  • 5 kudos

Functional Safetey U5 Series

in https://www.st.com/content/st_com/en/ecosystems/functionalsafety.htmlSTM32C0, F0, F1, F3, F4, F7, G0, G4, H5, H7, L0, L4/L4+, L5, U5, WL MCUs, STM32MP15 MPUit says U5 is included. in https://www.st.com/en/embedded-software/x-cube-stl.htmlAvailable...

STM32U545 External Loader "Init Function Fail"

I have an External Loader Project made for STM32G0/G4/L4.I ported it to STM32U5: all the functions work fine when debugged from STM32CubeIDE (so the connections are ok). With the STM32CubeProgrammer the .stldr file is recognized but the Read/Write/Se...

GiBi_01 by Associate
  • 5974 Views
  • 6 replies
  • 0 kudos

Resolved! Suggest a smaller STM32 IC for BMS application

Dear Sir/Madam,Good day~I am trying to build a custom PCB with an STM32 chip.Currently, NUCLEO-F439ZI Demo Board is used, but only few pins/functions of the STM32F439ZI chip are necessary for me, the used pins shown as below (20 out of 114 pins are u...

VinceTai_0-1738824445588.png VinceTai_1-1738826584242.png
VinceTai by Associate II
  • 2616 Views
  • 3 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.