STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

what is the maximum FSMC_CLK value for STM32F2 series?

Posted on April 21, 2017 at 14:49Hi,I am trying to set freq for FSMC, I am using STM32CubeMX for code generation.In clock configuration segment which clock is related with FSMC(is it APB1 peripheral clocks???).Please find the attached image file for...

Sensor MPU6050 with stm32

Posted on April 21, 2017 at 18:29Sorry! I have module  MPU6050 and STM32F103C8T6. I want to use it to get data but I don't know to work with them.Help me! Thank all :( 

Stm32f030f4p6 POR current problem

Posted on April 19, 2017 at 16:26Hi,I have designed low power detector with using stm32f030f4p6. In normal state detector is supplied with 24Vdc and it consumes 50uA. But when I supply the detector with 2V, mcu consumes 2mA. This high current consum...

stm32f429 rotary encoder external interrupt

Posted on January 05, 2017 at 10:43Hi,I am using rotary encoder with two input i/o and i want to read the encoder pinA and pinB values with external interrupt. I am using callback function for two input PA0 and PA1. My functions are below:In stm32f4...

er3481 by Senior
  • 1804 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F4 Camera with STM32F7 Discovery board?

Posted on February 19, 2017 at 20:59Hi all,I'm trying to use the camera STM32F4DIS-CAM with my STM32F7 Discovery board, with Keil uVision IDE. I have downloaded STM32Cube, and in the examples there is a BSP directory, with BSP drivers examples, incl...

Resolved! high voltage (80v) brushless motor control(FOC)

Posted on April 20, 2017 at 03:01Hello,What would be recommended to drive an 80V max brushless motor?I noticed all the integrated motor controllers are all relatively low voltage (45v max).  I would like to use the Nucleo-144 F7 series for this proj...

Resolved! Will an OFF state STM32 power up during SPI transaction

Posted on April 21, 2017 at 12:13We know a micro can be powered up using its GPIO. If you didn't know - https://www.eevblog.com/forum/blog/eevblog-831-power-a-micro-with-no-power-pin!/I have an STM32F0103 which will be in OFF state (VCC = 0 V) and a...

STM32F334 RTC Prescaler, Bug in Datasheet ?

Posted on April 17, 2017 at 19:36Hi,While trying to calibrate the RTC on the F334, tripped on this rather possible bug..I guess this is a bug in the Application Note AN3371Doc ID 018624 Rev 5Figure 11. Smooth calibration block, the RTCCLK is assumed...

How to enable RTC interrupt with HAL Library?

Posted on April 21, 2017 at 16:05Hi everyone,I'm using STM32F103 with CubeMX.I enabled the RTC Global Interrupt but I don't know how to configure it to generate a 1/4 second interrupt?Because the Reference Manual says:Three dedicated maskable interr...

ReV Hulk by Associate
  • 2085 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.