STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA only fetching 2 values from ADC

Posted on April 20, 2017 at 18:01STM32F437This is an update from my previous thread:https://community.st.com/message/154808-stm32f4-adcdma-always-returns-same-value The ADC2 DR has the right value in it but the DMA is not working as I thought it wou...

John Hite by Associate III
  • 2188 Views
  • 8 replies
  • 0 kudos

LwIP 2.0, how to build an SNMP agent

Posted on April 23, 2017 at 09:59Presently I am porting a project from the CooCox platform (lwip 1.4.1) to SW4STM32 platform (lwip 2.0). This portage is almost straightforward except for the porting of the SNMP agent.I do the portage on a STM32F4 bo...

STM32F4,DCMI_OV9655_SelectOutputFormat

Posted on April 21, 2017 at 00:02I am using the ov9655 camera for image processing with the STM32F4 microprocessor.  I want to convert the camera format from RGB to YUV(grayscala) . How can ı do it ?/* OV9655 Camera size setup */ #if defined (QQVG...

Strange points at ADC from STM32F407

Posted on April 22, 2017 at 16:17Hi, I am trying to use ADC with DMA on the STM32F407 in two channels (PA1 and PA2), so, basically I created the project using CubeMX, exported it to Coocox, ran the debug to fill the vector  and imported these points...

0690X00000606q2QAA.png

How transfer info from flash QSPI to SDRAM .

Posted on April 21, 2017 at 23:20HiI use STM32f779  and i have TFT LCD 800x480   controller tft is RA8875 .  I want to transfert my images to flash after i need to transfert to SDRAM  and transfert to controller RA8875 .   Can you help me how transf...

Resolved! Windows CDC Driver issue

Posted on September 02, 2016 at 08:34Hello.I want to use the USB High Speed with the class CDC in device mode. I am using the STM32F746G-DISCO board.I have created a project with STM32CubeMX , here there is the configuration : MiddleWare : USB DEVIC...

y23 by Associate
  • 3780 Views
  • 4 replies
  • 0 kudos

first time here - help with stlink programmer

Posted on April 22, 2017 at 00:54Hi there people!Ive got one big but a very basic question for yallIm just curious if following things are even possible and is this forum right place to find infoIve never ever been into this so know absolutely nothi...

MAC-layer of STM32F7

Posted on April 22, 2017 at 11:08Hi all,Problem with sending packet from MAC-layer of STM32F745VG to Physical Layer Transiver.ARP-packet is prepared to transfer after start. It is sent to Physical Layer Transiver in Evaluation Board (STM32746-EVAL2)...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.