STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 - STM8 Aerospace ?

Posted on April 11, 2017 at 08:27HiDoes anyone know if there are STM32 or STM8 availaible for aerospace apps ? I saw there were the RCP series for aerospace and defense apps ... but they are too much 'high-performance' for my app.Thank you ! Have a ...

Leo Leo by Associate II
  • 4437 Views
  • 6 replies
  • 0 kudos

STM32F103 - TIM1 PWM Interrupt not working?

Posted on April 17, 2017 at 17:56Hi, I'm using STM32F103RBTx MCU and I generate my code using CubeMX (v4.20.1).I need PWM output on 2 Pin: Timer1 - Channel 1 and Timer4 - Channel 4.These 2 PWM signal is used to control 2 separated DC motors.I config...

ReV Hulk by Associate
  • 2640 Views
  • 2 replies
  • 0 kudos

How can i use virtual com port in STM32F3 Discovery?

Posted on January 07, 2016 at 14:45HiToday, i bought a new cortex-m4 based STM32F3 Discovery.I was connect USB USER port to my notebook and i was waiting to recognize Virtual Com Port.But, my notebook didn't recognize STM32F3 Discovery.Fortunately, ...

FFT problem on stm32427- solved

Posted on April 20, 2017 at 16:11I have done fft computation but I got strange results.Please let me know if i did any mistake.why I am getting the following strange results?// ADC&sharpdefine ADC_RAW_LENGTH 512// FFT//&sharpdefine FFT_SAMPLES 2048&...

IDB05A1 working without jumper

Posted on April 21, 2017 at 10:17Hi,I am using a IDB05A1 board together with a L073RZ, is it normal that the IDB05A1 is working when i remove the J1 jumper?I don't get why since there's no connection between 3v3 and VDDThanks in advance Raphael

STM32756G-EVAL SPI/I2C

Posted on April 20, 2017 at 11:19HiI want to connect a thermal camera to the STM32756G-EVAL EV board.In order to connect it I need to have one free SPI terminal and one I2C free terminal.When looking at the user manual I can't find SPI mentioned any...

Convert SystemWorkbench to GNU ARM Eclipse ??

Posted on April 19, 2017 at 00:24I recently try to start a project using STM SensorTile which has the STM32L4 chip embedded.I have downloaded the STSW-STLKT01 and I have loaded coded using the AC6 SystemWorkbench, no problem.However, my boss need me...

STM32F7 multi-Slave SPI with CubeMX

Posted on April 21, 2017 at 03:14CubeMX 4.20.1STM32Cube_FW_F7_V1.6.1Target: STM32F765NIHxThe Reference Manual (RM0410 rev 2) Section 35.5.3 (multi-slave) Figure 390 Note 2 states that the MISO pins of all SPI Slaves must be configured as alternate-f...

Resolved! Accesing the field of a struct when it is a pointer?

Posted on April 20, 2017 at 19:39Having trouble reading the MAC address using the HAL but mostly because of my inexperience. uint8_t             *MACAddr;                   /*!< MAC Address of used Hardware: must be pointer on an array of 6 bytes */...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.