STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H563VIT6 DAC1 Output Unexpected

Driving DAC1 channel 1 with         HAL_DAC_Start(&hdac1, DAC_CHANNEL_1); ... while (1) { HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 4095UL); HAL_Delay(100UL); HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 0UL); HAL_D...

mccabehm_1-1738710940044.png mccabehm_2-1738711213554.png

Resolved! Trouble with ADC accuracy

I am using the ADC on a Nucleo-L412KB board.   I am setting up the ADC for  single conversion once per second. I am getting digital values which are off, as though the Vref is up around 3.4 V.  I have an LM385 voltage reference as a source and have t...

Clyde_S by Associate III
  • 15320 Views
  • 8 replies
  • 1 kudos

slow hspi clock speed on STM32U5G9

I am using the hspi1 peripheral in HyperBus mode on an STM32U5G9 processor.I used STM32CubeMX to configure the hspi clock to 160 MHz, generated from the SYSCLK.  The hspi is configured with 0 Clock Prescaler with the intention of having an external 1...

rdl_42 by Associate III
  • 1230 Views
  • 1 replies
  • 0 kudos

Program doesn't work anymore after ST-Link upgrade

 I had a program tested and running on a NUCLEO-F072RB for some time. Later I custom built my own PCB (using a STM32F072RBT6) and flashed the exact same code onto it using a STLINK-V3SET and the program did not work. I had no idea on why the program ...

Resolved! eStore coupon can't apply

Hi, I need help for estore coupon.  I got an email the redeem free board with exclusive code on ST estore.  After applying the code, A message "Your cart is not eligible for this promotion.  Ensure that you are logged in and items match promotion ter...

ctien1 by Associate
  • 2801 Views
  • 2 replies
  • 0 kudos

Resolved! ETH: anybody used KSZ8863RLL?

Heyho,until now I only used STM32 with the LAN8742, in a few weeks I'll get my 2nd custom board, but this time with the "dual" PHY KSZ8863RLL.It's connected via RMII, for setup MDIO (and optionally I2C for the registers not accessible via MDIO).Are t...

LCE by Principal II
  • 13735 Views
  • 23 replies
  • 8 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.