2025-01-20 1:53 PM - edited 2025-01-20 2:12 PM
I am using the ADC on a Nucleo-L412KB board. I am setting up the ADC for single conversion once per second.
I am getting digital values which are off, as though the Vref is up around 3.4 V. I have an LM385 voltage reference as a source and have tried a precision bench supply (Power Designs 2005) and with either input, working the math backwards, it is as though Vref is about 100 mV off.
I have read AN2834. This is a simple "get acquainted" exercise, with the board right out of the box.
Is there sometihng I could be overlooking? Am I required to set up Vref? Or is this handled by default with the HAL initialization?
Clyde
Solved! Go to Solution.
2025-01-20 8:39 PM
I think you need to include stm32l4xx_hal_adc_ex.h
its a bit different on the l4 than on the g0 im used to...
2025-01-20 4:30 PM
What is your setup physically? What is your vref source? Are you using the IDE to setup the ADC or are you setting it up yourself? Are you tried changing your vref value to verify that the ADC is using the vref that you think it is?
2025-01-20 4:40 PM - edited 2025-01-20 4:42 PM
I am using CubeIDE to set up the ADC. The analog input is fed by short jumper wires from my packaged Voltage Calibrator device. Vref is connected as the board comes, straight to AVDD.
I am attaching the initialization code:
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_MultiModeTypeDef multimode = {0};
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV64;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc1.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure the ADC multi-mode
*/
multimode.Mode = ADC_MODE_INDEPENDENT;
if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
{
Error_Handler();
}
2025-01-20 5:10 PM
What's your input impedance? What speed are you running your conversions at? Also, have you tried multiple conversions in a row and do they all come up with the same low value? Do you have any input filter since you do not seem to be doing any oversampling or averaging?
Also, are we talking about the raw number that the ADC captures? Or are you doing math on it first?
Have you called
HAL_ADCEx_Calibration_Start(hadcin);Prior to starting the sampling?
2025-01-20 5:24 PM - edited 2025-01-20 5:29 PM
I have tried two different input devices, the calibrator, which is a shunt regulator at 1.235 V, bypassed with 1 uF, IIRC. In reading other posts, it made me question the drive impedance, so I used the bench supply, adjustable to the 100 uV. Either test input is about the same.
The LSBs move around a bit, but if I do the math with 3.3 V as the value for Vref, it jumps around +1/-4 mV.
I think my input is very stable and quiet, so I don't think noise is the issue. I also tried the Nucleo-L4A6ZG and the same code, with the same result. (That is why I tried the L412KB.) I was convinced it was Vref, but I measured Vref=VADD=3.305 V. This is why I asked if I was missing something in the configuration. This should not be very hard to get correct, in my opinion. Thanks.
Oh, I cannot get the calibration function to compile.
2025-01-20 8:39 PM
I think you need to include stm32l4xx_hal_adc_ex.h
its a bit different on the l4 than on the g0 im used to...
2025-01-21 3:47 AM
Thank you. I believe you are correct in the include file is needed. I will give it a shot today.
Clyde
2025-01-21 4:04 AM - edited 2025-01-21 4:11 AM
That fixed it! I am maybe a little tiny bit noisy, and maybe a millivolt off, but those are my issues. I am on my way.
Thank you. A screen shot of my terminal is below:
L412KB Temperature Probe Calibrator.
Build: Jan 21 2025 07:01:25
Counts: 1528 Voltage: 1.231
2025-02-08 9:52 AM
A small update... I tried the oversampling today as my application is looking for accuracy, not speed, and it worked very nicely.
L412KB Temperature Probe Calibrator.
Build: Feb 8 2025 12:48:26
Counts: 24455 Voltage: 1.233 Low: 1.231 High: 1.234 Median: 1.233
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.