2026-03-16 7:28 AM - edited 2026-03-16 7:35 AM
Heyho,
I recently found that I'm not using ITCM RAM at all, then started to put heap and stack there.
No problems so far.
Then I copied some functions there, and all went well - until I found some strange behaviour:
Further info:
- instruction cache: in use
- data cache: not used
Is there any guideline what to put in ITCM, what are the limits, etcpp. ?
Solved! Go to Solution.
2026-03-18 2:44 AM
Hi @LCE
Few checks that might help narrow it down:
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-03-16 8:14 AM
... and yes, I checked AN4891, but that's more about benchmarks.
Not really clear about any requirements, but it looks like a function in ITCM doesn't have any restrictions about variable locations.
2026-03-16 2:02 PM
There are no restrictions with putting code into ITCM. It will run faster which can expose some bugs in the code, much the same as switching between Debug and Release can do.
Variables can't live in ITCM since it is dedicated for instructions. They are never put there in a normal workflow, you would have to be explicitly mixing code and data in the same section.
2026-03-17 12:15 AM
> It will run faster which can expose some bugs in the code,
> much the same as switching between Debug and Release can do.
This is something I actually like very much about Release / Debug / Optimization On/Off.
But in this case it's so crazy simple - but maybe there's something I just don't see. I'll go check once more...
2026-03-18 2:44 AM
Hi @LCE
Few checks that might help narrow it down:
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-03-18 4:57 AM
@FBL thanks, yes, there was a multiple DMA interrupt race condition.
I already used __disable_irq(); to prevent this, but in the callback it was "too late", as there's done too much in the HAL interrupt handler (which for DMA is one of the better / faster HAL interrupt handlers, which I usually avoid using).
Still need to have another look at it...
This way it works:
/* +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ */
/* SAI DMA interrupt handlers
* the global HAL_DMA_IRQHandler()
* - resets all flags
* - calls the half- / complete callback functions
*/
/* SAI 1 A as ADC */
void DMA1_Stream0_IRQHandler(void)
{
__disable_irq();
HAL_DMA_IRQHandler(&hDMA_Sai_1_A);
__enable_irq();
}
/* SAI 1 B as ADC */
void DMA1_Stream1_IRQHandler(void)
{
__disable_irq();
HAL_DMA_IRQHandler(&hDMA_Sai_1_B);
__enable_irq();
}
/* SAI 4 A as ADC */
void BDMA_Channel0_IRQHandler(void)
{
__disable_irq();
HAL_DMA_IRQHandler(&hDMA_Sai_4_A);
__enable_irq();
}
/* SAI 4 B as ADC */
void BDMA_Channel1_IRQHandler(void)
{
__disable_irq();
HAL_DMA_IRQHandler(&hDMA_Sai_4_B);
__enable_irq();
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.