2024-07-31 1:39 AM
hello, where can i download win11 STM virtual com port? i install both VCP_V1.5.0_Setup_w7_x64_64bits and W8_x86_32bit all not working ! i din see
STM Virtual Com port at device manager! only STM STLink visual com port appear ...
2024-07-31 1:56 AM
i m implementing my own USB VCP on a USB port (STM32 USB Virtual COM Port (VCP) )
https://medium.com/@pasindusandima/stm32-usb-virtual-com-port-vcp-bc7cb1bd5f5
2024-07-31 2:03 AM
i m using H734 Nucleo...
2024-07-31 2:23 AM
Hi,
the VCP driver :
https://www.st.com/en/development-tools/stsw-stm32102.html
should not be needed, as win10 + 11 have driver in system included - so maybe your enumeration going wrong...
or try thr driver - if you want.
2024-07-31 6:39 AM
yes, thats the website i downloaded, but STM Virtual Com port not appearing at device manager when plug usb cable into H743 Nucleo. Do you hav any idea what went wrong?
2024-07-31 7:09 AM
How should i know, what you doing ? (wrong or right...)
So verify you using a data cable, not a charger cable. :)
Then (which cpu ?) try a standard VCP , using HAL, just to see: it works - or not.
2024-07-31 7:49 AM
its data cable...not charger cable i m sure...wats try standard VCP ? i try this HAL la..
CDC_Transmit_FS((uint8_t *) charData, strlen(charData));
2024-07-31 7:51 AM
hello... anyone can help ???
2024-07-31 9:14 AM
Look for CDC device example in the Cube example projects for STM32H7, adapt it for your board.
2024-07-31 2:42 PM - edited 2024-07-31 2:43 PM
You don't need a VCP driver for late windows 8 forward. It just shows up as a COM port.
If your device isn't showing up, I'd suggest that there is something incorrect with your program running on the H7. You do have a program running on the H7, don't you? You have to provide a program that implements the device side of the VCP, it's not built into the H7.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.