USB Host Base Class 06h (Still Imaging) Â
Posted on May 19, 2017 at 11:30I need USB Host Base Class 06h (Still Imaging) ,Please Help.Ty.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on May 19, 2017 at 11:30I need USB Host Base Class 06h (Still Imaging) ,Please Help.Ty.
Posted on May 18, 2017 at 16:09Hello, I recently migrated from 8 bit processors and something that has always worked for me is showing some unexpected behavior. Clearly I am missing something very obvious to you 32 bit guys // define a structure som...
Posted on May 19, 2017 at 10:36I want to use the DSP library function 'arm_lms_f32'.My platform is Keil uVision5, it have a toolbox called 'Manage Run-time Environment'.I chose CMSIS/CORE, CMSIS/DSP, and Device/Startup.When I add the function into m...
Posted on May 17, 2017 at 16:52Hi everyone,Pretty new to WiFi I have some beginner questions:I want to build a small system using a STM32 that should connect to a smartphone using WiFi direct to upload/dowload pictures and other sort of documents.I'...
Posted on July 06, 2016 at 16:22Running the install SetupSTM32CubeMX-4.15.1.linuxcrashes. OS: Ubuntu 16.04LTS 64 Bitjava version:java -versionopenjdk version ''9-internal''OpenJDK Runtime Environment (build 9-internal+0-2016-04-14-195246.buildd.src)...
Posted on May 18, 2017 at 23:17I am working with the STM32F405 microcontroller and I have a an SPI-bus across a detachable cable (please no comments about this, it works fine and it's not the point of this post) and I'm using the DMA-controller to b...
Posted on May 17, 2017 at 12:50HI, not much experice with Cortex Devices,Is there any Software Interrupt Example, for M0/M0+ devices.I am using STM32 Cube's HAL structure, with a F091 Nucleo board.Just found a void SVC_Handler(void) in the stm32f0xx...
Posted on May 17, 2017 at 18:38Hello,I am working with the board P-NUCLEO-LRWAN1 (https://community.st.com/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fen%2Fevaluation-tools%2Fp-nucleo-lrwan1.html) for a project. I want to add a GPS receiver to ...
Posted on May 17, 2017 at 18:30How can I wirte algorithm for power spectral density and spectrogram?Thank in advance #power-spectral-density #fft-stm32f4 #spectogram
Posted on May 16, 2017 at 23:35To run multiple STM32F7's as SPI Slaves I enable/disable their active control of MISO using:/* Enable MISO to be actively driven (i.e., controlled by the SPI2 module). */GPIO_InitStruct.Pin = SMCU_SPI2_MISO_Pin; GPIO_I...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.