USBH_Process but no user code area - I'm on the wrong track?
Posted on May 20, 2017 at 03:44The original post was too long to process during our migration. Please click on the attachment to read the original post.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on May 20, 2017 at 03:44The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on March 15, 2017 at 19:19Hello,I am now using STM32F042F6P6 for control purpose on my gate driver board. However, the ambient temperature requirement is changed to 120C compared to 85C before.Since STM32F042F6P6 can not work under this temp...
Posted on May 18, 2017 at 20:28I'm using STM32Cube_FW_L4_V1.6.0 for long bulk transfers (up to 4096 bytes). When the stm32 receives a packet longer that 64 bytes, HAL_PCD_EP_GetRxCount returns a number 1-64 (e.g. a packet of 1024 returns a lengt...
Posted on May 19, 2017 at 15:26Hi,We have X-NUCLEO-IDS01A4 and tried to access the EEPROM by assembling R3. But unable to do it.Please provide any sample code.
Posted on May 19, 2017 at 13:38Hi there,I am using STM32F207VET and I have successfully Implemented Ethernet as TCP echo server(MII Full Duplex only).I have successfully connected my module with 5 clients over LAN and Exchanged data between them.A...
Posted on May 18, 2017 at 11:40Οn which documentation file can one find the address mapping for the ARM registers on topic?
Posted on May 17, 2017 at 19:26The highlight color of a selected function for a pin is dark blue with black text. That means it is impossible to read whatever it says. It seems to have been this way for a while. Do the programmers of STM32CubeMX nev...
Posted on May 19, 2017 at 12:28Hi,I am working on STM32F769BIT MCU. I have parallel 24 bit RGB data enable mode LCD Display.I have generated a code from STM32 CUBE and changed the settings related to PIN,PORT configurations related to R[0-7],G[0-7],...
Posted on May 18, 2017 at 17:34Hey,I have recently bought the CJMCU-407, but I'm not able to let any LED blink... does anyone can help me out there? #stm32f4 #cjmcu #pin-map
Posted on March 09, 2017 at 22:58We're having problems at the moment getting our device (STM32F405ZGT6) to enter DFU mode, or rather, we can enter it, but it always takes a little over 2 minutes to appear. We have a push button switch to on the boar...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.