2017-05-17 9:38 AM
Hello,
I am working with the board P-NUCLEO-LRWAN1 (
) for a project. I want to add a GPS receiver to that board for the purpose of that project . Can you tell me which one I should choose ? And how difficult is to get NMEA data ?
Thank you in advance
2017-05-17 9:55 AM
I'm using the DISCO board, but a shield like this should suffice. On the Nucleo-64 D0/D1 has some conflict with the ST-LINK VCP but you might have other pin choices
Removing link for Duinopeak GPS Shield NEO-6M to break the moderation on this post..
NMEA data starts automatically at 9600 8N1, connect it to a few USART input.
2017-05-17 2:42 PM
http://www.ebay.com/itm/Duinopeak-NEO-6M-GPS-Shield-for-Arduino-with-GPS-Antenna-/272137634759
2017-05-18 1:50 AM
NMEA data starts automatically at 9600 8N1, connect it to a few USART input.
I know boards that use a different default baudrate. Just check the manual.
Usually, the baudrate can be switched at runtime, and NMEA sentences can be turned on/off.
2017-05-18 10:27 AM
Some older GPS were 4800 baud (think 1980's era designs/compatibility), but the data stream typically generated in the last decade overwhelms that.
Both the NEO-6M and NEO-M8N, and similar variants, all support 9600 baud by default, but can be reconfigured
YMMV, but always RTFM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.