2017-05-17 7:52 AM
Hi everyone,
Pretty new to WiFi I have some beginner questions:
I want to build a small system using a STM32 that should connect to a smartphone using WiFi direct to upload/dowload pictures and other sort of documents.
I'm looking for a wifi module that uses SDIO also, as I want to be at full speed, serial to wifi module would be easier to uses but I don't want to be limited by the UART speed.
I was thinking about using a LILY-W1 module from u-blox as it does WiFi direct.
So, using this kind of module, do I have to code a WiFi stack for the STM32 by myself ?
does the LwIP TCP/IP stack is suitable for SDIO WiFi module ? can I do WiFi direct from it ?
thanks,
Thomas.
2017-05-17 11:32 AM
https://forum.u-blox.com/index.php?qa=10857&qa_1=stm32-and-lily-w1
I suspect the biggest complication would be the use of the SDIO peripheral on the STM32 in this fashion, and if you can find anyone with direct/relevant experience there.
The STM32 can sustain some pretty high baud rates on short on-board connections between modules.
ST just announced a low cost Cortex-M4 based WiFi part, 2MB of FLASH, running Micro Python.
http://blog.st.com/spwf04-low-power-wi-fi-micropython-applications/
2017-05-17 3:03 PM
Hum ok I see, thanks.
2017-05-18 11:52 AM
Or find a wifi module with AT command set witg spi support. Driving directly a wifi rf front end will be challenging if malfuncting when coexisting with the application.
2017-05-18 11:54 AM
After some research, it as been done before obviously.
As it is how the WICED module / particule photon is made.
https://docs.particle.io/datasheets/photon-datasheet/
http://www.usish.com/english/products_wiced.php
A wifi tranceiver connected to a STM32 via SDIO for WLAN, and I bet this is how SPWF01/04 are made too, and all other same kind of wifi module.
while these are powerful tools if used as stand alone like the
SPWF04 can be
, they often miss some interfaces and GPIO that I need for ma applications:(
.2017-05-18 11:57 AM
I guess that will be my choice yes, but I will have to downgrade my network speed expectation as with SPI I'll never reach 50+Mbps for data transfers.
2017-05-18 12:22 PM
These things are prevalent on eBay, just don't know how much of the stack you have access too, and if it offer the modes desired.
https://www.seeedstudio.com/EMW3162-WiFi-Module-p-2122.html
2017-05-18 6:56 PM
Which application?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.