STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PA13 and PA14 how do i make these GPIO outputs

Posted on June 19, 2017 at 07:43I am using a custom STM32L051xxx, I want to change these two programing ports to PP outputs.I think I need to DeInit them then apply the normal Init procedure, I cand see how to DeInit these ports.ThanksKevin NZ

CubeMX Pin Speed Bug

Posted on December 01, 2016 at 17:01Hello,we are using a stm32f4 with a LTDC Display. CubeMX set's the speed of all Pins to LOW. Same problem with the MCO Pin.I hope this information will help you improve your products.Yours faithfully #!stm32-!c...

tekampe by Associate II
  • 3147 Views
  • 5 replies
  • 0 kudos

STM32F4 unwanted wakeup PA0

Posted on June 18, 2017 at 15:07Hi,Using an STM32F446.I setup PA0 to exit from standby mode.The first time I enter StandbyMode, it works well, and I can exit from standby mode by using PA0.But the next time entering standby mode, the STM32 automatic...

Kuikui by Associate III
  • 1269 Views
  • 1 replies
  • 1 kudos

Minimum DAC output Voltage on stm32f30x

Posted on June 17, 2017 at 11:47Hello,What is the minimal voltage the DAC can output?When I read the Datasheet for the stm32f301 I can see a min of 0.2V with buffer ON.However when the buffer is OFF the manual says 0.5mV.I use the DAC internally as ...

STM32F030 PROGRAMMING

Posted on June 17, 2017 at 18:12Hi all,with uvision5 I'd make a project that works in debug, but when I program the flash of STM32 the adc peripheral doesn't works. I use Nucleo-64 board.Any suggestion?Thanks 

sav gas by Associate II
  • 3020 Views
  • 6 replies
  • 0 kudos

HASH: mixed feeding it with DMA and non-DMA writes possible?

Posted on October 31, 2015 at 15:55When I feed HASH with regular writes only or DMA only, everything is OK. But I need to use both methods when computing hash of a long message, and in this case I cannot manage to compute right hash value. Did anybo...

our by Associate II
  • 3684 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.