2017-06-18 6:07 AM
Hi,
Using an STM32F446.
I setup PA0 to exit from standby mode.
The first time I enter StandbyMode, it works well, and I can exit from standby mode by using PA0.
But the next time entering standby mode, the STM32 automatically wakes-up from standby without any action on PA0 ( stays at 0 ).How can this be ?
The code I use for entering standby mode is :
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);
PWR_BackupAccessCmd(ENABLE); RCC_BackupResetCmd(ENABLE); RCC_BackupResetCmd(DISABLE); PWR_WakeUpPinCmd(PWR_WakeUp_Pin1, DISABLE);PWR_ClearFlag(PWR_FLAG_WU);
/* Check if the StandBy flag is set */
if (PWR_GetFlagStatus(PWR_FLAG_SB) != RESET) { /* Clear StandBy flag */ PWR_ClearFlag(PWR_FLAG_SB); } PWR_WakeUpPinCmd(PWR_WakeUp_Pin1, ENABLE); PWR_EnterSTANDBYMode();Thanks for help.
Best regards,Vincent.
#stm32f4-wakeup2017-06-19 2:20 AM
ok, I got the point.
There's a mistake in SPL library :
void PWR_ClearFlag(uint32_t PWR_FLAG)
{ /* Check the parameters */ assert_param(IS_PWR_CLEAR_FLAG(PWR_FLAG)); #if defined (STM32F427_437xx) || defined (STM32F429_439xx) if (PWR_FLAG != PWR_FLAG_UDRDY) { PWR->CR |= PWR_FLAG << 2; } else { PWR->CSR |= PWR_FLAG_UDRDY; }#endif /* STM32F427_437xx || STM32F429_439xx */#if defined (STM32F40_41xxx) || defined (STM32F401xx) || defined (STM32F410xx) || defined (STM32F411xE) || defined(STM32F412xG)
PWR->CR |= PWR_FLAG << 2;#endif /* STM32F40_41xxx || STM32F401xx || STM32F410xx || STM32F411xE || STM32F412xG */}STM32F446 users like me have been forgotten !!
So I've done it manually : PWR->CSR |= 0x0000000C; <= to clear WU and SB flags
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.