2016-12-01 8:01 AM
2016-12-05 2:19 AM
Dear User,
Thank you for highlighting this. Your feedback is shared internally for further review.
All comments and suggestions are welcome to improve our products.
Best Regards
-Imen-
2016-12-05 9:35 AM
Speed is really rise or fall time of the pin.
2017-05-04 8:02 AM
Hi
Tekampe.Jens
,Sorry for the late reply.
Yes, indeed, the maximum output speed for all LTDC pins is set to Low. And you can modify this speed to set your own speed.
You have an example in figure 39 in the
. For me, here is no issue and no enhancement here to add.If I misunderstand something, do not hesitate to reply on this post.
BR. Eric
2017-05-04 1:13 PM
Defaulting to low toggle speed is definitely the right way for CubeMX.
That reduces unnecessary high frequency contents in the signals and thus minimizes possibly unwanted EMC issues.
2017-06-19 9:34 AM
Hi
Roehrig.Valentin
,generally i'm on your side, but the LCD-Displays are working at several MHz. So you have to turn it to high speed.
Or are there displays with low speed which i don't know about?
Thanks for the help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.