STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Brown out and flash read potection in F410

Posted on June 20, 2017 at 17:23BOR_LEV and RDP fields seems to be duplicate: both appears in option bytes and in FLASH_OPTCR. Are they alias to each other? If option bytes and FLASH_OPTCR differs in these fields which setting is applied?Can Option ...

RTC Time value

Posted on November 28, 2016 at 10:59Hi, I'm using STM32L476RG microcontroller and I'm configuring the RTC to get the instant time value. I'm using LSE with 32,786 KHz as a clock source for my RTC . I have followed this application note (http://www.s...

STM32 RTC Digital Smooth Calibration

Posted on June 20, 2017 at 16:36 Hi everybody, I've got a custom made board with STM32L486VG on it. I'm trying to do a RTC calibration with external 1Hz clock based on http://www.st.com/en/embedded-software/x-cube-rtc.html. Everything is set...

jan by Associate II
  • 1108 Views
  • 0 replies
  • 0 kudos

SDRAM layout on an STM32F427 with 4 x 512Mb

Posted on June 20, 2017 at 14:23Hi Everyone,I want to use the STM32F427VIT6 controller with four SDRAMs (IS42S86400D) and I would like to get some information of schematic and layout design. The address bus would be connect directly. Data bus would ...

Attila _ by Associate
  • 940 Views
  • 0 replies
  • 0 kudos

Which stm32 is best for making a CAN network log?

Posted on June 20, 2017 at 10:09I would like to build a project based on STM32 that interfaces with a CAN network. The CAN network has a 250kbps baud rate.On this network I have to: Log messages from 127 nodes with IDs between 0x381 and 0x3FF (Each...

Timer encoder overflow interrupt

Posted on June 20, 2017 at 06:31Hi All ,   I am interfacing a quadrature encoder to TIM4 in the Encoder Mode using STM Cube with STM32F103. I set up the timer and configure the counter to counter till 1000. The function HAL_TIM_IC_CaptureCallback() ...

Resolved! No Errorflag when writting to Write-Protected Sector

Posted on June 14, 2017 at 14:46 Hi, I'm evaluating some flash functionalities of the STM32F469NI. I have configured the Sector 12 of my STM32F469 Flash (2MB) with a Write-Protection. When I debug my Firmware I see that the corresponding bit g...

andi z by Associate II
  • 1503 Views
  • 2 replies
  • 0 kudos

Resolved! HTIM UIF clear from capture callback

Posted on June 19, 2017 at 15:26On a STM32 F777 I am configuring TIM4 to read Hall sensors (HAL_TIMEx_HallSensor_Init).I have enabled capture interrupt and in capture callback  (which is triggered at every Hall event as expected) I am clearing UIF f...

Can I program STM32F042C6T6 via STM32F0DISCOVERY?

Posted on June 20, 2017 at 08:10I am gonna use ST uM's for the first time. What I need is the simplest and cheapest PIC with CAN-BUS connectivity. So I found this: https://www.digikey.com/product-detail/en/stmicroelectronics/STM32F042C6T6/497-14648-...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.