STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Confusing about Sram

Posted on June 27, 2017 at 10:53Please give me some time to describe the problem I met, please give me some advice or comments. The http://www.kynix.com/uploadfiles/pdf65976/STM32F030C8T6.pdf is also given below.Source Program is given below:       ...

[STM32F4] Compile

Posted on June 27, 2017 at 11:13Hello.Can anyone compile this project for me? https://github.com/vanbwodonk/STM32F4_USB_MP3

ST-link v2 at 1.8V?

Posted on June 26, 2017 at 17:37I am using the ST-Link v2 with a target STM32 board running at 1.8V. I connect the 'target Vcc' to my boards Vcc ok, but the SWDIO and SWDCLK outputs from the ST-link are at 3.3V. Yet it looks like it is supposed to w...

Looking for the latest document AN2606

Posted on June 26, 2017 at 22:27I guys,I'm looking for the latest version of the application note: AN2606 (STM32â„¢ microcontroller system memory boot mode). I have a 2013 version.  Where can I find it?Thanks. Francois.

STM32F746ZG+PHY+LwIP+Interrupts mode +without os

Posted on February 10, 2017 at 08:59we are working on STM32F7 nucleo 144 board.we are successfully tested the LWIP+POLLING MODE with the help of example STM32Cube_FW_F7_V1.6.0\Projects\STM32756G_EVAL\Applications\LwIP_Tcp_Echo_Client.we are using cu...

Em R by Associate
  • 1365 Views
  • 1 replies
  • 0 kudos

TIM_Input_Capture_Prescaler effect

Posted on June 26, 2017 at 22:15What is the effect of TIM_Input_Capture_Prescaler on the value of the CNT counter in the encoder mode, even if I change this value between TIM_ICPSC_DIV4 or TIM_ICPSC_DIV1 the reading of the CNT is the sameI use nucle...

Write multiple GPIO pins on the same port

Posted on June 25, 2017 at 17:04My code is written in C and I am using your HAL library I need to set/Reset 6 GPIO pins on the same port now I iam doing it by calling 6 times to HAL_GPIO_WritePin which take too much time how can I do it in one cpmma...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.