STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F051x programming system memory

Posted on June 27, 2017 at 10:02hi everyone,i�m working with the STM32F051.I want to programm the System memory over the Serial interface using the ST Flash Loader Demonstrater.So i set the BOOT0 Pin high, and connected the STM32F051 to the Computer...

ST-LINK/V2 with Low Power mode

Posted on June 27, 2017 at 16:06With our custom board (STM32F103) i debug with Segger J-Link. No Problem with 'WFI' instruction.Now i tried to use ST-LINK/V2 with latest firmware (2-28). Download and single step actions are ok, but in run mode the a...

Configuring GPO on the M24SR

Posted on June 27, 2017 at 13:57I am controlling the M24SR from a STM32F030R8 over I2C, trying to configure it so the GPO pin is triggered by the SendInterrupt command over RF. I have been working from the example code given http://www.st.com/en/eco...

STM32H7 maximum timer frequency

Posted on June 26, 2017 at 17:14Hello,the STM32H743 datasheet is out. I think the datasheet disaggrees on 'Max timer clock'. Table 4 in footnote 1 tells that 400 MHz is possible depending on  the TIMPRE bit, while electrical characteristics 6.3.31 T...

Where can I get the firmware for STEVAL-ISV003V1?

Posted on June 27, 2017 at 11:59Dear Imen D,where can I get the firmware for STEVAL-ISV003V1? Because, currently I worked on a solar micro-inverter based on STEVAL-ISV003V1 and cannot find any reference about the firmware for that product.

ade by Associate II
  • 1116 Views
  • 1 replies
  • 0 kudos

STM32Cube versus STD_peripheral

Posted on March 30, 2016 at 15:01Hi all,I have been working with ST for many years but the Cube software might make me move to a different brand! The Cube might be nice for newbies but it is a PAIN for people like me who need to push the micro's to ...

Resolved! Template bug in startup_stm32f030x8.s file (v1.6.0)

Posted on September 29, 2016 at 10:20After some debug work (erratic but constant jumps to the Hard Fault ISR), I discovered an error in one of the .s template files contained in the STM32Cube_FW_F0_V1.6.0 package:The ISR vector for Timer6 is missing...

giocc by Associate
  • 1611 Views
  • 2 replies
  • 0 kudos

[STM32F4] Help in compile

Posted on June 27, 2017 at 09:16Hello.Can anyone compile this project for me?I am a beginner and I upload a variety programs on the board for training. However, with this project I have a lot of trouble...Thank you in advance.

Resolved! STM32F103C8 board bring up

Posted on June 20, 2017 at 14:08Hi All,I am new to this domain. I am using STM32F103C8 controller and has some proprietary OS on it.My objective is:1. To understand aspects(Hardware, Software, Tools, Memory etc) to be considered to add new OS.2. To ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.