STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F779xx startup issue with HardFault Exception

Posted on May 31, 2017 at 03:52Hello.I seem to have a hardfault exception problem and it doesn't make sense to me.I am using ThreadX and it has to do with how long it takes to startup.So here is my startup code:/* Enable I-Cache---------------------...

netstv by Associate II
  • 1421 Views
  • 1 replies
  • 0 kudos

target halted due to breakpoint

Posted on June 22, 2017 at 02:37Hello, I'm a new with STM32.I have Nucloe-N053R8, Win8.1, SystemWorkbench.I made a short program and it seems that I could send the program to the Nucloe-board, but it doesn't work. I can see the console said 'target ...

stm32f103c8t6 STM32CubeMX 4.20.1 usart

Posted on June 26, 2017 at 17:56Hello,i wanted to know if there any probleme when using usart with stm32f103c8t6 with a project configured using STM32CubeMX 4.20.1,Because after the configuration i tried to send an uint8_t variable with the value 0x...

sak hos by Associate III
  • 753 Views
  • 0 replies
  • 0 kudos

SRAM2 Differences Between L433 & L452?

Posted on June 07, 2017 at 05:11I have been fighting with a problem for the past few days as I port a board over from an STM32L433CC to an STM32L452CE.  Code that runs fine on the L433CC causes a hard fault on the L452CE.  After quite a bit of effor...

Using Interruption without Delay

Posted on June 26, 2017 at 13:17Hi community !,I'm using STM32f1031RB Nucleo 64, and I wanted to know how can I programm my timer TIM2 (internal clock), in order to allow some of interruptions in my main programm. Actually; I'm using HAL_Delay and I...

Resolved! Which memory can be used for periph to mem transfer?

Posted on June 23, 2017 at 16:05Hello,I use the CPU STM32F765.I want to use DMA2 to transfer ADC-results into memory.This works fine if I use DTCM-Memory for the destination  (128kbyte  from 0x20000000 to 0x2001ffff)If I use SRAM1, DMA seems to work...

Set/Reset multiple GPIO pins in one port

Posted on June 26, 2017 at 08:53I asked this quiestion yesterday and for some reason I do not see it in the forum ans also did not got any email about it.I want to Set/Reset 6 GPIO pins belong to the same port using HAL what I am doing now is callin...

STM32F746 USB Host examples do not work with vars in SRAM1 ?

Posted on August 31, 2016 at 14:16Hi,Using the CubeF7 USB Host examples ok with default provided linker script (using SW4STM32 SystemWorks IDE).Yet, when moving the .bss & COMMON section out of the DTCM RAM region into the SRAM1 RAM region, example ...

sv1eia by Associate II
  • 1175 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.