Can STM32CubeMX add the BSP when generating code?
Posted on January 16, 2017 at 15:19Is there a way to get STM32CubeMX to add the BSP when it generates code?
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on January 16, 2017 at 15:19Is there a way to get STM32CubeMX to add the BSP when it generates code?
Posted on July 14, 2017 at 15:41Hello,in my STM32F765 project I am using a timer (TIM6) which is set to a constant frequency. The update event of the timer triggers an ADC (ADC2&3) which is configured to start conversion of a regular group of channe...
Posted on July 17, 2017 at 09:24My Environment:STM32F042 Nucleo-32 dev board which has STM32F042K6T6 MCU of 32pin QFPKEIL ARM MDK v5Host Windows 10 OS The BOOT0 pin PB8 is not available on the CN3 or CN4 connector. I've used the below code and it i...
Posted on July 16, 2017 at 22:56Hello, Hope you are fineIs there a sample project to play mp3 files from MMC using Hal functions?MCU : STM32F103
Posted on July 15, 2017 at 20:56The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on March 17, 2017 at 02:14Hello.I want to know more specification of STM32H7 series.But, Information was not in ST site.So I want to get datasheet and reference manual for STM32H7.If it is possible to share, could you open more information.I ...
Posted on July 15, 2017 at 18:36I'm using the STM32107 and want to use application code to activate the STM32 bootloader in system memory. I've consulted the AN2606 Application Note where it states...'In addition to patterns described above, user ca...
Posted on July 13, 2017 at 16:59Dear members of ST community,I have a firmware that is runs perfectly on a L072Z -LRWAN1 discovery board, but the program stops working when activating RDP level 1. I tried removing the stlink jumpers and load the hex...
Posted on July 15, 2017 at 16:09Hello.I am using STM32F746BG. I use FreeRTOS and USB CDC class code.when I create an IAR Project using STM32CubeMX, USB com port correctly identify by windows but can not open.but if i change code like cod below, it w...
Posted on July 15, 2017 at 11:06I am using the STM32F411 as an I2C master to control a DC_DC converter with PMBus support.This device is within a local system, and it allows all 128 addresses to be assigned with seven user-assignable address pins. S...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.