STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC can't work because PLL already use

Posted on July 17, 2017 at 07:46Dear Sir:I had reference the PWR_STANDBY_RTC sample code form STM32Cube_FW_L4_V1.8.0This sample code are work well and wake up about 30 second,but after move to my code get return fail atif(HAL_RCC_OscConfig(&RCC_OscI...

Resolved! HAL I2C Communication Problem

Posted on July 14, 2017 at 11:52Dear Sir/Madam,I am working on STM32F405 mcu.I developed my code on cubemx and HAL drivers.I want to interface microchip adc 'MCP3428' via HAL I2C drivers but unfortunately i was failed.Anybody of you please help me t...

HAL Documentation PDF Table of Contents

Posted on July 14, 2017 at 23:26Would it be possible to make the table of contents in the HAL Documentation PDFs more useful? Currently it looks like this:It would be way more useful if section 49.2 had headings in the table of contents for each fun...

0690X00000607YtQAI.png

Confused on TIM_SelectCCDMA

Posted on July 14, 2017 at 15:19I want to use Timer Capture event to generate DMA requests, how TIM_SelectCCDMA should be called?TIM_SelectCCDMA(TIMx, ENABLE)?This will set CCDS bit, but according the reference manual for STM32F303, bit CCDS should ...

USB HID keyboard

Posted on July 17, 2017 at 12:48How to turn On/Off leds on keyboard conected by usb/hid interface? Keyboard is working in BOOT mode

STM32L071 : adjust RTC prescaler when using LSI

Posted on July 17, 2017 at 09:24Hi, My projetct using RTC based on LSI : I've see a code example where the TIM21 Input Capture of TIM_CHANNEL_1 is connect internally to the LSI clock output; to mesure periode and ajust prescaler (STM32Cube_FW_L0_V1....

STM32F7 1.6.1 package broken

Posted on April 11, 2017 at 14:21Missing a whole bunch of LWiP files as well as stm32f7xx.hIt is supposed to be a patch, but STM32CubeMX just uses it instead of 1.6.0OS: macOS 10.12.4

aa aa by Associate
  • 1164 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.