2017-07-16 10:46 PM
Dear Sir:
I had reference the PWR_STANDBY_RTC sample code form STM32Cube_FW_L4_V1.8.0
This sample code are work well and wake up about 30 second,
but after move to my code get return fail at
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) form
SystemClock_Config()void SystemClock_Config(void)
{......
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLP = 7; RCC_OscInitStruct.PLL.PLLQ = 4; if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {// return here.while(1);
}after check, find is because PLL already used?
/* Check if the PLL is used as system clock or not */
if(__HAL_RCC_GET_SYSCLK_SOURCE() != RCC_CFGR_SWS_PLL) {.......
else
{ return HAL_ERROR; }I have reference this web say need turn off some content of
SystemInit()
https://www.mianbaoban.cn/blog/post/45024
but still don't work, then how to use PLL and let SystemClock_Config?
Thx for your answer.
2017-07-17 2:37 AM
Hello
Normaly after reset (wkup reset after stby mode) the MSI is the default clock source .
check the standby flag after reset to see if the mc was in StandBy Mode.
__HAL_PWR_GET_FLAG(PWR_FLAG_SB);
Clear this flag after read it.
2017-07-17 4:49 AM
thx for reply.
at the sample code,
int main(void)
{
HAL_Init();
SystemClock_Config();
BSP_LED_Init(LED2);
RTC_Config();
SystemPower_Config();if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET) {__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); }.....
I do the same thing, but return error from
SystemClock_Config();
I have try move clear sb flag to up then SystemClock_Config(), but get same result.
BTW, my project is base on zephyr RTOS.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.