STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC Accuracy - STM32L475

Posted on August 29, 2017 at 14:43According to pre-fixed parameters when setting up the RTC (PREDIV_A=127m PREDIV_S=255) and in accordance with AN4759, if I use a reccomended 32.768KHz (LSE) crystal, I should have a 512Hz signal at PC13 pin (STM32L4...

STM32F103 Assembler Interrupt Handling

Posted on August 30, 2017 at 11:16 Hello community, Iwould like to configure Timer 2 of my STM32F103C8 to use it as a simple overflow interrupt service and Iwould like to do this in assembly language. On page 198 of the reference manual i f...

loder by Associate II
  • 1444 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F303ZE Reference Manual clarification needed.

Posted on August 24, 2017 at 22:04HelloI'm about to start a project and the STM32F303ZE seems like a perfect part. I was reading through the Reference Manual and I found in the section 15.3.11 Channel selection (SQRx, JSQRx) that the ADC1 is connect...

m4l490n by Senior
  • 1390 Views
  • 2 replies
  • 0 kudos

Stm32f103 Flash size

Posted on August 30, 2017 at 13:06Hi,Actually i am using STM32F103VBT6, But now my code exceeds 128KB.So with out changing my circuit can i use any of other Controllers of STM32F103 series which has more flash size and package should be LQFP100.Fast...

Resolved! 2 Channel PWM with STM32L

Posted on August 30, 2017 at 11:26Hello,I'm using Murata's LoRa module which has STM32L inside.http://www.murata.com/en-global/products/lpwa/loraThis module's timer related output is,- PB5/LPTIM1_IN1- PB6/LPTIM1_ETR- PB7/LPTIM1_IN2- PB2/LPTIM1_OUTNo...

Jay Kim by Associate
  • 1278 Views
  • 1 replies
  • 0 kudos

TIM5 TixFPx needs ~50mA to GND

Posted on August 29, 2017 at 21:07Hello, I'am trying to use the TIM5 in Slave-(and Master-)Mode to drive another Timer (TIM1 to Trigger a DMA-Request on each Period).When I configure TIM5 in Triggermode TI2FP2 on Stm32F4Discovery Board (PA1 and this...

andre23 by Associate II
  • 2125 Views
  • 4 replies
  • 0 kudos

STM32 as quadrature encoder output

Posted on August 29, 2017 at 10:02 Hi everyone, I need to reed a quadrature encoder signal from a sensor, modify the number of pulse and send this signal out to a machine. The output signal must be a TTL quadrature signal, I have 5 pins: 0v, 5v...

paul sauv by Associate III
  • 5826 Views
  • 12 replies
  • 0 kudos

STM32 resetting on first sdram access

Posted on August 29, 2017 at 10:09Good morning, I have a STM32F429 based board, the MCU is interfacing a Micron SDRAM (MT48LC4M32B2). We successfully configured the sdram interface using the FMC driver. We use 1.4.3 version.We had a first production...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.