STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32Cube L4 firmware v1.8.1 patch issue

Posted on July 24, 2017 at 05:43STM32CubeMX v4.22 fails to merge L4 v1.8.1 patch with existing L4 v1.8.0 source tree. Instead it creates two distinctive trees, one for v1.8.0 and one for v1.8.1 when they are installed one after another, i.e. when yo...

Innomatic by Associate II
  • 4491 Views
  • 11 replies
  • 0 kudos

STM32F469I Discovery - cannot flash demo hex file

Posted on January 12, 2017 at 14:59Hi,I'm trying to flash the demo hex file from STM32F469I-Discovery Kit. But STLink Utility fails when download the Firmware.I've attached log Files.Following Error Message occurs:14:32:53 : Connection to device is ...

Resolved! STM32L4 hard faulting in BlueNRG stack

Posted on August 03, 2017 at 20:25Hi,   I am building an application using an STM32L4 and a BLUENRG-MS.  I have an GATT server application that can happily connect and ping pong messages with a GATT client.  The client sends a ping on one characteri...

HAL_CAN_ErrorCallback

Posted on August 31, 2017 at 15:01What to do to leave the error state of the state machine?Calling HAL_CAN_DeInit() and HAL_CAN_Init() does not do the job.#hal_can

LP-Timer problems

Posted on August 31, 2017 at 14:19I am using the ST32L476 and found out the following:1. The LP-Timers don't generate a compare-interrupt when the value of the CMP-Register is 0x7FFF, all other values are working correctly.2. Writing to the CMP-Regi...

What Happened during while() loop?

Posted on August 30, 2017 at 13:05 I recently noticed a strange case on STM32F7 I measure the execution time of this function by clock cycles. which is just a simple while loop. void LK_ADDr(float *im, float *meanParameter, int Size ) { ...

0690X0000060813QAA.png 0690X000006084eQAA.png 0690X000006084jQAA.png

Resolved! ADC VDDA and PA2 measurement

Posted on August 30, 2017 at 15:46Hello Community,I work on a STM32L151CCU6 and I need your help.I try to measure VDDA voltage in order to calculate a voltage divider on PA2 (single mode). My two ADC configuration functions are :void MX_ADC_Init(voi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.