2017-08-30 6:46 AM
Hello Community,
I work on a STM32L151CCU6 and I need your help.
I try to measure VDDA voltage in order to calculate a voltage divider on PA2 (single mode). My two ADC configuration functions are :
void MX_ADC_Init(void)
{ GPIO_InitTypeDef gpioInit1; GPIO_InitTypeDef gpioInit2; gpioInit1.Pin = PID_PIN; //PA2 gpioInit1.Mode = GPIO_MODE_ANALOG; gpioInit1.Pull = GPIO_NOPULL; HAL_GPIO_Init(PID_PORT, &gpioInit1); PA2 gpioInit2.Pin = PID_POWER_SUPPLY_PIN; //PB2 gpioInit2.Mode = GPIO_MODE_OUTPUT_PP; gpioInit2.Pull = GPIO_NOPULL; HAL_GPIO_Init(PID_POWER_SUPPLY_PORT, &gpioInit2); //PB2 __HAL_RCC_ADC1_CLK_ENABLE(); ADC_ChannelConfTypeDef sConfig;/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/ adc_identification.Instance = ADC1; adc_identification.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2; adc_identification.Init.Resolution = ADC_RESOLUTION_12B; adc_identification.Init.DataAlign = ADC_DATAALIGN_RIGHT; adc_identification.Init.ScanConvMode = ADC_SCAN_DISABLE; adc_identification.Init.EOCSelection = ADC_EOC_SEQ_CONV; adc_identification.Init.LowPowerAutoWait = ADC_AUTOWAIT_DISABLE; adc_identification.Init.LowPowerAutoPowerOff = ADC_AUTOPOWEROFF_DISABLE; adc_identification.Init.ChannelsBank = ADC_CHANNELS_BANK_A; adc_identification.Init.ContinuousConvMode = DISABLE; adc_identification.Init.NbrOfConversion = 1; adc_identification.Init.DiscontinuousConvMode = DISABLE; adc_identification.Init.ExternalTrigConv = ADC_SOFTWARE_START; adc_identification.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; adc_identification.Init.DMAContinuousRequests = DISABLE; if (HAL_ADC_Init(&adc_identification) != HAL_OK) { while(1); }/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/ sConfig.Channel = ADC_CHANNEL_2; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_384CYCLES; if (HAL_ADC_ConfigChannel(&adc_identification, &sConfig) != HAL_OK) { while(1); } ADC_Enable(&adc_identification);}and :
void MX_ADC_VDD_Init(void)
{ ADC_ChannelConfTypeDef sConfig; /**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)*/VDD_measurement.Instance = ADC1;
VDD_measurement.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1; VDD_measurement.Init.Resolution = ADC_RESOLUTION_12B; VDD_measurement.Init.DataAlign = ADC_DATAALIGN_RIGHT; VDD_measurement.Init.ScanConvMode = ADC_SCAN_DISABLE; VDD_measurement.Init.EOCSelection = ADC_EOC_SEQ_CONV; VDD_measurement.Init.LowPowerAutoWait = ADC_AUTOWAIT_DISABLE; VDD_measurement.Init.LowPowerAutoPowerOff = ADC_AUTOPOWEROFF_DISABLE; VDD_measurement.Init.ChannelsBank = ADC_CHANNELS_BANK_A; VDD_measurement.Init.ContinuousConvMode = DISABLE; VDD_measurement.Init.NbrOfConversion = 1; VDD_measurement.Init.DiscontinuousConvMode = DISABLE; VDD_measurement.Init.ExternalTrigConv = ADC_SOFTWARE_START; VDD_measurement.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; VDD_measurement.Init.DMAContinuousRequests = DISABLE; if (HAL_ADC_Init(&VDD_measurement) != HAL_OK) { while(1); }/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/ sConfig.Channel = ADC_CHANNEL_17; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_4CYCLES; if (HAL_ADC_ConfigChannel(&VDD_measurement, &sConfig) != HAL_OK) { while(1); } ADC_Enable(&VDD_measurement);}When I try to measure this two ADC channel, I find 0.
I use this function : HAL_ADC_GetValue(&VDD_measurement);
Does anyone know where is my problem?
Thanks,
Jérémy
Solved! Go to Solution.
2017-08-31 1:41 AM
For some reason the post is doubled.
this is the yesterday's answer
2017-08-31 1:41 AM
For some reason the post is doubled.
this is the yesterday's answer
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.