STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F4xx_StdPeriph_Templates missing file

Posted on September 05, 2017 at 16:11Dear All,Currently I've just got a STM32F429ZIT6 Discovery kit from ST.Q1. I'd like to exam the simple gpio firmware into my kit. So I open the STM32F4xx_StdPeriph_Templates  project in Keil. But I come across th...

0690X000006044VQAQ.jpg

Resolved! Why does STM32F4 Discovery kit

Posted on September 05, 2017 at 14:03Hi,I've just got a STM32F4 Discovery kit (STM32F429)I thought that it embedded software for demonstate at the first time.But my kit does not work.I also I read the below instruction.But I don't know should I have...

STM32H7 maximum sdram frequency

Posted on September 05, 2017 at 10:37The STM32H7 series drive SDRAM by fmc,Which is maximum sdram frequency 100Mhz or 200Mhz can run?There are four input clock sources for fmc_ker_ck, and SDRAM clock can be fmc_ker_ck/2 or fmc_ker_ck/3.If I choose c...

0690X000006087sQAA.png
HAN Wu by Associate
  • 3088 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMX: Problems installing new libraries

Posted on February 13, 2017 at 11:52I am using STM32CubeMX Version 4.16.1 on a pc without(!!!) internet access.I would like to install a new library via 'Menu'/'Help'/'Install New Libraries'/'From Local...'.I have downloaded the firmware package for...

Tob G by Associate II
  • 3593 Views
  • 6 replies
  • 0 kudos

STM32F7 dual bank random RWW stalls

Posted on June 28, 2017 at 11:13Hello everyone,I am having very weird problem using RWW functionality on STM32F767VIT6. I have searched through various places and found no hints to my issue. Any pointers are welcome.My flash organization is followin...

how should i handle httpd_cgi_handler()?

Posted on September 05, 2017 at 16:58Hi there!new LwIP stack given by STM32Cube calls httpd_cgi_handler() from httpd.c file. Unfortunately i could not find any docs or examples on how to use this hande (i.e. how to make my own CGI processing).Any he...

stm32l053 adc multiple channel without DMA

Posted on September 05, 2017 at 14:24Hi,                I'm trying to read 2 number of ADC channels on stm32l053 without DMA by initializing channel 1, reading  & deinitializing channel 1 then initializing channel 2, reading  & deinitializing channe...

LRPS_92 by Associate II
  • 872 Views
  • 0 replies
  • 0 kudos

STM32f4 Bluetooth Module

Posted on September 05, 2017 at 12:43Hi,I'm trying to connect STM32f407VG with Bluetooth module and light the led on and off. I'm a beginner and i get really confused all these things. I'm using Keil and CubeMX.I found a code for STM32F10x but I can...

Icube_LRWAN ( End_node)

Posted on September 05, 2017 at 12:15Hello , i'm using murata's module CMWX1ZZabz including stm32l0,  with the provided lorawan_cube code , here is the lowpower_handler fontion, anyone has an idea how to control the MCU wakeup.in addition to that, t...

Kim ElQ by Associate II
  • 648 Views
  • 0 replies
  • 0 kudos

STM32F765 Ethernet stop working increasing MCU clock

Posted on September 01, 2017 at 17:37Hi All,     I am working on a custom board using the STM32F765.The ethernet peripheral is based on DP83620 connected in RMII. In my application the ethernet is working as the AHB clock is below 190MHz, then it st...

raffin by Associate III
  • 1694 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.