2017-06-28 2:13 AM
Hello everyone,
I am having very weird problem using RWW functionality on STM32F767VIT6. I have searched through various places and found no hints to my issue. Any pointers are welcome.
My flash organization is following:
The trouble I am having is when I am upgrading application during runtime. The simplified process is following:
Problem is following: Sometimes the whole MCU freezes during the erase phase. This happens like 20% of time. These freezes range from approximately 150ms to over 1s. This of course forces the watchdog to reset the whole MCU.
How is that possible? The whole dual bank concept is designed to allow RWW without any stalls at all. The weirdest thing is, that it happens only from time to time. I flash 5 times in a row without any issue and during the sixth attempt I get the stall and MCU restarts.
Thank you for your time.
Tomas
#stalling #dual-bank #stm32f767-iap2017-06-28 3:03 AM
Hello
tomas
,up to 1second takes time to erase sectors. My questions are these:
Keep in mind that when you execute code from bank (let's say bank 1) and if you also erase/write/read this part, execution will slow down because of memory matrix designed on STM32F7.
To get maximal performance, erase memory from another bank (eg. erase app1 from bank 2 and app 2 from bank 1).
2017-06-28 3:45 AM
Hi Tilen,
thanks for quick reply.
All flash erase/write operations are done in application code. App1 is erasing/writing app2 and vice versa.
2017-09-05 8:26 AM
Hello
Tomas, did you solve this problem?
I see same issues on a STM32F765VGT. I have it configured in dual bank mode. The application code in BANK1 erase BANK2 and most of the times MCU freezes until erase is finished, but not always. No code what I can see is accessing BANK2 during the time. I have also setup the Memory Protection Unit to detect acceses to BANK2 areas and it dosent trigger.
Best regards
Stefan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.