STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 dual bank flash erase stall

Posted on September 06, 2017 at 13:53HelloI am using STM32F765VGT and have the flash in dual bank configuration.I have an application in bank1 erasing bank2. Most of the times, but not always, the processor stalls during erase of bank 2. I dont do a...

Resolved! STM32F429-disc1 GPIO_IOToggle test (How can I modify GPIO pin

Posted on September 05, 2017 at 18:43Hi.I've done set up the \STM32F4xx_DSP_StdPeriph_Lib_V1.8.0 with keil and  think the flash download works good.So I'm trying to implement GPIO_IOToggle test with STM32F4xx_DSP_StdPeriph_Lib_V1.8.0's  template pro...

0690X000006044fQAA.jpg

Can I mask NRST signal input temporarily?

Posted on September 05, 2017 at 18:12Hi there,I am coding STM32F030F4 using CubeMX generated EWARM project. All ICs are monitored by single voltage supervisor including F030, but unfortunately one of IC has design problem and it need a 'reset pulse'...

yoshi by Associate II
  • 2336 Views
  • 5 replies
  • 0 kudos

Resolved! Counting Rising Edge

Posted on September 06, 2017 at 10:11Hello I  use STDPERIPH_DRIVER .I want Counting a pulse and when it arrive to special number (100 Rising edge) I get an interrupt.How can i do that?I do somthing like that TIM_ICInitStructure.TIM_Channel = TIM_Cha...

Return value from CMSIS osSemaphoreWait

Posted on December 17, 2015 at 10:40 According to the http://www.keil.com/pack/doc/CMSIS/RTOS/html/group___c_m_s_i_s___r_t_o_s___semaphore_mgmt.html#gacc15b0fc8ce1167fe43da33042e62098(CMSIS version 1.02) the return value should be the number ...

soren2 by Associate
  • 1928 Views
  • 2 replies
  • 0 kudos

STM32F042 Nucleo USB detect connection and disconnection

Posted on September 02, 2017 at 14:55Hi all,i have a problem with STM32F042 Nucleo and USB Connect detection.I made my own MIDI Interface with CUBEMX (generated a CDC Projekt and changed it with help from some internet sites to MIDI) and it works we...

hans23 by Associate II
  • 3130 Views
  • 5 replies
  • 0 kudos

STM32Cube_FW_L4_V1.8.0\Projects\STM32L432KC-Nucleo\Examples\PWR\PWR_STANDBY_RTC example project

Posted on September 01, 2017 at 19:36Hi I just purchased the STM32L432 Nucleo board  and tried to run the example from the folderSTM32Cube_FW_L4_V1.8.0\Projects\STM32L432KC-Nucleo\Examples\PWR\PWR_STANDBY_RTCI found that I could not find the definit...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.