2017-09-18 8:58 AM
Hello, my problem is I need to acquire a waveform at high frequency (sampling frequency in the order 35 to 50 MHz carried out by fast external ADC). I would like to use an high performance STM32 microcontroller (such as F3 or F4) to acquire 8 bit digital inputs (ADC output) and transfer them to memory by DMA however I do not know what is the maximum frequency for the operation'DMA read input port and transfer to memory'.
Anyone can help?
Thanks.
2017-09-18 9:11 AM
The DCMI port is supposedly capable of 54 MHz operations, but you'll be hard pressed to consume/process data at such rates. How deep of a sample buffer are you looking at?
FIFOs can also be used from high rate capture
http://www.averlogic.com/AL422B.asp
2017-09-18 9:22 AM
The analog signal is 6.78 MHz and is sampled by an external pipelined fast ADC (50 Msps). What I need is to acquire the ADC 8 bits digital outputs with a STM32 input port and transfer the byte to memory. If I use a 48Mhz clock for ADC then I can acquire about 7 samples per period. I think a buffer of 70 bytes (10 periods) should be enough.
Naturally sampling with higher frequency would provide more samples per period but I have no idea how to do it.
2017-09-18 11:51 AM
At 48 MHz you need to be looking at the DCMI peripheral and how to utilize that.
If you use the FIFO device, you could access that via the FSMC/FMC
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.