STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743 Rev. Y and system memory

Posted on September 05, 2017 at 10:13Hello,by chance I got hold of a NUCLEO-H753ZI board. Using STLINK V2J28M18, I can read memory and flash as expected. But reading system memory at 0x1ff00000 gives 'Device Memory not accessible'. As another indica...

Resolved! Error Correcting Code (ECC) in STM32L4

Posted on September 22, 2017 at 10:32Hi,I have a question which i'm not able to find an understandable answer in the datasheet. The STM32L4 seems to have an Error Correction Code function embedded inside its Flash memory.According to an ST powerpoin...

STM32F103 External Switch Interrupt Problem

Posted on September 21, 2017 at 11:41My aim is to generate interrupts on various pins of STM32F103 Nucleo-64, for that i used these steps as mentioned bellow , In cubeMx firstly i used 5 pins which are connected to switches and configured them as GP...

touch sense TSC documentation

Posted on February 07, 2017 at 12:10Hiwhere do I see which STM32 has how many TSC channels? In this document: UM1913 User manual: Developing applications on STM32Cube with STMTouch� touch sensing librarySTM32L083VBTx is not listed!But in STM32CubeMX...

How to design a TSC pcb layot?

Posted on June 07, 2017 at 14:26Hi, I'm working on TSC whit STM32F051,  I 'm going to desing TSC pcb layot, i read the AN4312, that explain how to design, but doesnt include details. My the must problem is about shielding. For example what is Driven...

stm32F051 Touch TSC with cubeMX

Posted on November 20, 2014 at 10:33 Hello, i try to develop a touch interface with the stm32f051 and want to use the stm32CubeMX Software. I want to do it with an interrupt and have the generated code in my IAR. My question is, where i c...

uli by Associate II
  • 2174 Views
  • 4 replies
  • 0 kudos

i can't get work accelerometer

Posted on March 17, 2017 at 10:14Lis2dh connect with stm32l151 on i2c bus.function initial i2c:I2C_DeInit( I2C1 ); RCC_APB1PeriphClockCmd( RCC_APB1Periph_I2C1, ENABLE ); RCC_AHBPeriphClockCmd( RCC_AHBPeriph_GPIOB, ENABLE ); GPIO_PinAFConfig( GPIOB...

ST-Link VCP on Nucleo-144 STM32F767ZI Configuration

Posted on September 21, 2017 at 16:34I am trying to use STM32CubeMX V4.22.1 with the F7 package V1.8.0 to configure USART3 which connects to the ST-Link VCP. Here are my issues:1. Does the ST-Link processor autobaud to detect the USART3 configured s...

MDS by Associate III
  • 2000 Views
  • 4 replies
  • 0 kudos

How can I temporalily detach/reattach the MSC only portion of a Composite USB MSC + HID Device from the device itself?

Posted on August 17, 2017 at 21:49I have a USB Composite MSC + HID device running on an STM32F746NG (DISCO board) and using an SD card as the local storage. The device also has a local FAT file system accessing the same SD card. I want to be able to...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.