2014-11-20 1:33 AM
Hello,
i try to develop a touch interface with the stm32f051 and want to use the stm32CubeMX Software. I want to do it with an interrupt and have the generated code in my IAR. My question is, where i can found a tutorial/dokumentation how to implement a scan which touchbutton is pressed. I found a lot for TSL (Library) but not for TSC which use the library but use other functions/names. I think the treshhold voltage is initializise in the init-function so i have in the interrupt only to check if a IO is high or low. I have the code for the Touch sensing interrupt:void TSC_IRQHandler(void){
} I've found this post:
/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Touch%20Sensing%20on%20STM32F0&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=1340
The point is, i don`t know the syntax i need to scan my input like:if (button_1){ ..} PA0 and TSC_G1_IO1 aren't known in my project but stands as comments in the TSC.c.
Can anyone give me a tip or a link?
#touch-tsc-f0
2014-11-21 1:55 AM
I don't understand your problem, but if it is Cube-related, you should post it in the dedicated ''Software tools'' sub-forum.
https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx JW2014-11-21 4:15 AM
Hy,
My problem is the C-code for the µC.i have 12 touch buttons and i want to differentiate which button is pressed.It is a very simple problem but i don't know how it's work and didn't find the explanation. Maybe the problem is to simple for an document...Can i use something likeif(GPIOA->IDR & (1<<PinNr))
?I haven't the PCB yet and have to predevelop the software so i can't test it.I searched in sources like touch library, stm32f051 datasheet, stm touch driverI'm starting to feel like an idiot...2014-11-21 4:30 AM
Ok, i've found the
STMicroelectronics: Reference Manual of STM32F05xxx advanced ARM-based 32-bit MCUs
I think that is what i needed...STMicroelectronics: Reference Manual of STM32F05xxx advanced ARM-based 32-bit MCUs STMicroelectronics: Reference Manual of STM32F05xxx advanced ARM-based 32-bit MCUs STMicroelectronics: Reference Manual of STM32F05xxx advanced ARM-based 32-bit MCUs
STMicroelectronics: Reference Manual of STM32F05xxx advanced ARM-based 32-bit MCUs STMicroelectronics: Reference Manual of STM32F05xxx advanced ARM-based 32-bit MCUs STMicroelectronics: Reference Manual of STM32F05xxx advanced ARM-based 32-bit MCUs
STMicroelectronics: Reference Manual of STM32F05xxx advanced ARM-based 32-bit MCUs STMicroelectronics: Reference Manual of STM32F05xxx advanced ARM-based 32-bit MCUs STMicroelectronics: Reference Manual of STM32F05xxx advanced ARM-based 32-bit MCUs
2017-09-22 12:00 AM
my problem too
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.