STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4xx NVIC->ISPR Question

Posted on September 23, 2017 at 16:27When is the ISPR register used?ISPR [0] | = 0x00000001 << 6; // (EXTI0 Position)Does this code convert the EXTI0 interrupt into the pending state so that the EXTI0 interrupt should not be executed?But the interru...

0690X00000608LpQAI.png

trigger timer with external pulse...

Posted on September 22, 2017 at 23:14hi i need start timer with external pulse at falling edge at one pin and i need stop timer with external pulse at falling edge at one pin can convert two 16 bit timer to one 32 bit timer ?on stm32f103c8t6 my time...

stm32l4 CubeMX touch sense

Posted on August 30, 2016 at 11:56Hi,I'm trying to figure out, how to use the CubeMX generated project for touch sense aplication. I'm able to detect the change on the 3 touch buttons, but i can't figure out, how to detect on which touch button did ...

I/O Mirroring

Posted on September 26, 2016 at 16:23I need to simply capture an input level and then output the same logic level as soon as possible on another pin.This can be simply done with EXTI, but I was wondering if there is a passive peripheral based soluti...

Noise levels in ADC in STM32L4?

Posted on September 19, 2017 at 23:41I have a custom board using an STM32L452. I'm doing some testing of the ADC and am finding pretty high levels of noise.I have a rail-to-rail op amp driving the ADC pin with a 300 ohm resistor from the amp to the ...

DAC noise on SDCARD reads - SOLVED

Posted on September 03, 2017 at 23:44I have a custom board (2 layer) using a STM32F446RETx (3.3v) with STM32CubeMX, V4.22 with firmware V1.16.0.  I am reading/processing MP3 files from a sdcard and there is a low-level but perceptible 'thump' in the...

0690X000006086LQAQ.png

I2C READ NO RESPONSE

Posted on September 23, 2017 at 07:34Dear All,I am configuring I2C for reading EEPROM address.I am using PB6_I2CSCL and PB7_I2CSDA pin and have connected EEPROM AT24C A2,A1 and A0 pin to GND. I have written following code to read the EEPROM but i am...

STM32L0 Stop Mode Not Working Properly

Posted on September 23, 2017 at 20:16 Hello, Currently, I am working on optimizing current consumption by using STOP Mode of the STM32L053C6T6 processor. I'm facing a problem that I can not get through, and I'm very happy if you can help. ...

STM32L4 Serial audio interface

Posted on September 08, 2017 at 14:46Hello,I want to implement an audio record based on STM32L4. To do that  I want to use the SAI peripheral. By Referring to the STM32L4 datasheet the SAI don't support a microphone interface. So, in such case shall...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.