2017-09-22 10:34 PM
Dear All,
I am configuring I2C for reading EEPROM address.
I am using PB6_I2CSCL and PB7_I2CSDA pin and have connected EEPROM AT24C A2,A1 and A0 pin to GND.
I have written following code to read the EEPROM but i am unable to read the data.Please suggest me if am missing something in configuration or in reading part.
#define EEPROM_ADDRESS 0xA0
/* USER CODE BEGIN 3 */
ui8TxData[0]=0x00; ui8TxData[1]=0x31; ui8TxData[2]=0x32; ui8TxData[3]=0x33; ui8TxData[4]=0x34; HAL_I2C_Master_Transmit(&hi2c1,EEPROM_ADDRESS,ui8TxData,5,50); HAL_I2C_Master_Receive(&hi2c1,EEPROM_ADDRESS|0x01,&ui8RxData[0],1,50); HAL_I2C_Master_Receive(&hi2c1,EEPROM_ADDRESS|0x01,&ui8RxData[1],1,50); HAL_I2C_Master_Receive(&hi2c1,EEPROM_ADDRESS|0x01,&ui8RxData[2],1,50); HAL_I2C_Master_Receive(&hi2c1,EEPROM_ADDRESS|0x01,&ui8RxData[3],1,50); HAL_I2C_Master_Receive(&hi2c1,EEPROM_ADDRESS|0x01,&ui8RxData[5],1,50); HAL_Delay(100);Thanks in advance
Rohit
2017-09-23 2:14 PM
Hello!
The appropriate function to read from I2C EEPROM is HAL_I2C_Mem_Write(..) (also in IT and DMA version)
https://community.st.com/0D50X00009XkW1qSAF
is a relative post andhttps://community.st.com/0D50X00009Xke3SSAR
is anotherregards
vf
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.