STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

External Loader for STM32H533RE with W25Q32

Hi,I try build loaders for STM32H533RE using its nucleo board but it fails to read any thing using the cube programmer. i tried with nucleo H753 and it worked. i see that u already did loader for the H5 so would u please explain how or maybe update y...

msalem88 by Associate II
  • 2253 Views
  • 6 replies
  • 0 kudos

Resolved! STM32 HyperRAM Memory access issue

Hi,I am starting a new post for visibility, hopefully someone can point me towards the right direction.The setup:MCU: STM32H725HyperRAM: W957A8MFYA5I, /CK is groundedOCTOSPI1 is used, its reference clock is 200MHz, so with the Clock Prescaler I am us...

kacsaaa_0-1740502754143.png
kacsaaa by Associate II
  • 1385 Views
  • 1 replies
  • 0 kudos

ADC doesn't work

Hi all, I have created a new project for the STM32U575RIT6 microcontroller using the attached .ioc file. On top of the auto-generated code, I have made the following modifications:In main.c:    while (1) { uint32_t bits = 0; uint16_t adc_value =...

proyo by Associate II
  • 1466 Views
  • 3 replies
  • 1 kudos

Resolved! Own custom build STLDR file creation issue

hi,I am trying to build my own STLDR file with STM32H723ZGT6 + w25q128.I could able to build the stldr file STLDR creation with Separate Project 1 but it's not working with external loader  project 2 it's giving down load error while program download...

MMARI.1 by Senior II
  • 2562 Views
  • 5 replies
  • 0 kudos

Resolved! Spi clocks are 4, 5, 6 instead of 8 bits

Hi allI am using the stm32h743 device when using spi 6 to transmit data the clocksare 4, 5, 6 randomly instead of 8 bitswhen configuring spi2 the processor function perfectly.on this device I have already used connection: SPI1, SPI5, ethernet, uart4....

dorong by Associate II
  • 5087 Views
  • 17 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.