STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 SRAM DOUBT

Posted on October 26, 2017 at 15:57I'm using STM32F0 Discovery and need to store values in SRAM when MCU is powered off.I already removed SB1 shunt. Then VBAT is not powered from VDD but pin3 of P1 (VBAT pin supplied with 3V).When I turn off my STM2...

jmpo by Associate
  • 2050 Views
  • 4 replies
  • 0 kudos

Stm32f4 discovery dac ouput play

Posted on November 08, 2017 at 07:32how can I play two speaker by stm32f4 discovery board?how can I use both DAC (dac1 and dac2) output to play the speaker?  

mohit rai by Associate II
  • 1587 Views
  • 2 replies
  • 0 kudos

STM32L4 Oversampler producing odd results

Posted on November 09, 2017 at 23:59STM32L496CubeMX v4.21  (Edit, updated to V4.22.1, same issue)HAL Framework: 1.8I'm trying to reduce some of the noise in my system by using the hardware oversampling.  However, I've noticed that the resulting conv...

Jim Kaz by Associate II
  • 1848 Views
  • 3 replies
  • 0 kudos

Problem in external interrupt on PORTB

Posted on November 07, 2017 at 06:31I am using STM32F0308 Dicovery Board. I want to use external interrupt on PIN11 of PORTB. Problem is that I am not able to invoke the PORTB. Microcontroller is still uses PIN11 of PORTA. I know that pins of ports ...

PWM Generating Problem

Posted on November 10, 2017 at 09:52hii have a problem in pwm.i want to generate a pwm signal by nucleo stm32f103rb board,i use keil for the compiling,and i don't get the pwm.this is my code :&sharpinclude <stm32f10x.h>TIM_TimeBaseInitTypeDef TIM_st...

ADC Interrupt

Posted on November 10, 2017 at 07:28I have used STM CubeMX and Keil u5 and i have interfaced a Potentiometer with Nucleo  STM32F103RB Devkit so i am getting  ADC Values using  these function,  ' HAL_ADC_Start_DMA(&hadc1,ui32ReadADCBuffer,3);    ui32...

STM32L4 UART behaviour

Posted on November 10, 2017 at 09:29Hi,In the application I'm currently working with, it is possible to have several devices (UART controlled) but it is not known if the device is connected or not. I use USART3, UART4, UART5. I measure each USART/UA...

FMC clock limitation described on DS12117

Posted on November 10, 2017 at 07:30Hi,While I was reading DS12117(which is the data sheet of STM32H753xI), I discovered something is different with STM32F7 description.On the description of memory feature, they say Flexible external memory controll...

stm32f207 develop flash and memory log write help!

Posted on November 10, 2017 at 04:46Hello !!stm32f207 I am trying to develop on a Nucleo board.Receive an alarm message ([2017,01 / 15 16:07 20] AC Power OFF) from uart,Write and read to Flash and then write the recorded log dataI want to create a t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.