2017-11-09 10:28 PM
I have used STM CubeMX and Keil u5 and i have interfaced a Potentiometer with Nucleo STM32F103RB Devkit so i am getting ADC Values using these function,
'
HAL_ADC_Start_DMA(&hadc1,ui32ReadADCBuffer,3);
ui32Pot1 = ui32ReadADCBuffer[0];
ui32Pot2 = ui32ReadADCBuffer[1];
ui32Pot3 =
ui32ReadADCBuffer[2];
'But Is there any way where i can read the ADC values only when the potentiometer(POT) is rotated means do we have any callback fuction for it to interrupt the flow of code once the Potentiometer(POT) values are changed
Like if intially the POT position is stable i will not read ADC values but when i rotate or change the POT value i should a callback or interrupt then i will perfor these instructions '
' ui32Pot1 = ui32ReadADCBuffer[0]; ui32Pot2 = ui32ReadADCBuffer[1];ui32Pot3 =
ui32ReadADCBuffer[2];
'
I got one function but i am not able to get the exact use or functionality of that function please check with this function and also if there is any other way i can achieve the above told interrupt please let help me.
2017-11-09 10:29 PM
I have used STM CubeMX and Keil u5 and i have interfaced a Potentiometer with Nucleo STM32F103RB Devkit so i am getting ADC Values using these function,
'
HAL_ADC_Start_DMA(&hadc1,ui32ReadADCBuffer,3);
ui32Pot1 = ui32ReadADCBuffer[0];
ui32Pot2 = ui32ReadADCBuffer[1];
ui32Pot3 =
ui32ReadADCBuffer[2];
'
But Is there any way where i can read the ADC values only when the potentiometer(POT) is rotated means do we have any callback fuction for it to interrupt the flow of code once the Potentiometer(POT) values are changed
Like if intially the POT position is stable i will not read ADC values but when i rotate or change the POT value i should a callback or interrupt then i will perfor these instructions '
'
ui32Pot1 = ui32ReadADCBuffer[0];
ui32Pot2 = ui32ReadADCBuffer[1];
ui32Pot3 =
ui32ReadADCBuffer[2];
'
I got one function but i am not able to get the exact use or functionality of that function ( 'HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc1)' )please check with this function and also if there is any other way i can achieve the above told interrupt please let help me.
2017-11-10 12:51 AM
But Is there any way where i can read the ADC values only when the potentiometer(POT) is rotated means do we have any callback fuction for it to interrupt the flow of code once the Potentiometer(POT) values are changed
No.
And actually, you don't want that.
The ADC value will always have some noise, two or three bits at average. How will you discern such value changes (noise) from potentiometer turns ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.