2017-11-07 10:32 PM
how can I play two speaker by stm32f4 discovery board?
how can I use both DAC (dac1 and dac2) output to play the speaker?
2017-11-08 3:43 PM
There is an example of using DAC in [STM32Cube_FW_F4_V1.16.0]\Projects\STM32F4-Discovery\Examples\DAC\DAC_SignalsGeneration\. It's just one channel but may provide a starting point if you use Cube. Note that you cannot connect speaker directly to DAC output pin, as it's relatively high impedance; you'll need to add a high input impedance power amplifier.
JW
2017-11-10 3:51 AM
hello,
Thank you for your response. I have used lm386 amplifier circuit. Now, it is working.
Regards,
Mohit rai
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.