Batch unique ID programming
Posted on November 14, 2017 at 13:19Hi,I have 100 units that I need to program with unique ID, SN... somewhere in the FLASH memoryWhat is the easiest way to do it?Thx,Michael
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on November 14, 2017 at 13:19Hi,I have 100 units that I need to program with unique ID, SN... somewhere in the FLASH memoryWhat is the easiest way to do it?Thx,Michael
Posted on November 14, 2017 at 12:55vera.laurent &sharpSTM32 &sharpdisco-l072 I am new to STM32 and using SM32L072CZ discovery board with LoRa, Can someone please share the AT_Slave code in 'MBED'.null
Posted on November 14, 2017 at 10:47 Hello there, with my STM32F103, I'm working with the M25P40 SPI flash memory. With cube32Mx I configured the SPI3 with Chip Select (NSS) hardware and I perform Read/Write/WriteRead operation with Interru...
Posted on November 14, 2017 at 14:30I have recently completed a project to write a password manager using the stm32f469i-discovery board and would now like to take it on the road with me but am having a problem finding a suitable enclosure to protec...
Posted on March 07, 2017 at 11:48Hi We are using X-NUCLEO-IDB05A1. Why EEPROM is used in the board.
Posted on November 14, 2017 at 04:36Dear All,I'd like to implement FFT within STM32F103C8 without any extra memory buffers.So I want to know how many memories are needed to implement if I have 2592x1944x8bit size's one image?
Posted on January 11, 2017 at 15:21I am trying to interface a Teknic Clearpath SDSK motor to STM32F7 Nucleo Dev Board. It is a Brushless DC motor with a stepper like interface. The motor moves a set distance based on the number of pulses it receives...
Posted on November 13, 2017 at 12:59How can I use 'stm32f4xx_hal_uart_emul.c' driver in STM32F303CC MCU ? http://www.st.com/en/embedded-software/stsw-stm32156.html Please help in porting/using this Software UART driver in STM32F303CCWhat all change...
Posted on November 12, 2017 at 01:01Hello Folk!I checked all the demos, projects, templates, whatever, inside the Cube package for F4 devices but couldn't find anything similar to the F4 demo builder package. Audio playback layer in particular. Asid...
Posted on October 31, 2017 at 04:53Hi, I am using an STM32L053xx in StandBy mode for 500ms and Run mode for 2ms. I have noticed in StandBy my PCB draws about 120u amps more after the SW-DB has been connected.To correct this I need to disconnect the...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.