2017-11-13 4:29 AM
I have a problem with PWM generation.
I have my own PCB with the uC STM32F429IIH. I am trying to configure the PWM in TIM3 channel 1. My clock frecuency is 180 MHz and APB1 Timer Clock is 90 MHz.
I use STM32CubeMX to initialize the board. In the timer 3, I configure the prescaler with value 5 and the period with value 4095, so my PWM signal frecuency must be 3.66 KHz. Furthermore, I configure a fixed pulse of 500. In the main function I call the function HAL_TIM_PWM_Start to start the PWM signal.
In an oscilloscope I observe that the frequency is correct but the duty cycle is unstable. Most of the time, duty cycle varies between 12.2% and 12.3% but sometimes it downs till 11.6%. It seems that in some cycles the duty cycle changes too much.
I have tried to change the duty cycle, the prescaler and the period, but I always have the same problem: the duty cycle is unstable. I have tried with another oscilloscope too.
Does anyone know why the duty cycle varies so much? Am I configuring something wrong?
Thanks for your help.
#stm32f4-pwm #pwm #pwm-unstable #duty-cycle2017-11-13 6:32 AM
For fine granularity get the prescaler to zero (DIV1), and do all the division in the period.
If you suspect the source clocks output them via PA8 (MCO), to look at HSE and PLL clocks. I wouldn't expect HSI to be terribly stable.
2017-11-13 6:55 AM
How are you measuring your duty cycle?
If you are just reading off what your scope is giving you, the most likely explanation is that the instability is just the scope's inaccuracy, it's only in the order of +/- 0.5%.
Try to determine the accuracy of the duty cycle measurement.
2017-11-13 8:07 AM
It is only a 3 KHz signal, on presumably a 10+ MHz scope
2017-11-13 8:25 AM
Yes, but if there's too few samples per period (too many periods squeezed into the sampling window) then the granularity error will be way more than the sample timing error.
JW
2017-11-13 9:03 AM
Several orders of magnitude to play with though, assuming it's not some 1Msps POS
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.