STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32l476 how i can write 32bit data to internal flash

Posted on November 17, 2017 at 16:08Hi!!I worked before them on this crystal stm32f0, stm32f1 series. Recording to the internal flash memory was not a difficult process, which made it fun to work. Why did you make it so complicated, why record 64-bi...

den2life by Associate II
  • 2886 Views
  • 5 replies
  • 0 kudos

Stm32f302 interface with lcd (NHD-0420H1Z-FL-GBW-33V3)

Posted on November 18, 2017 at 20:42Hello everyone, I am trying to interface stm32f302r8t6 to LCD (NHD-0420H1Z-FL-GBW-33V3) here is datasheet  http://www.newhavendisplay.com/specs/NHD-0420H1Z-FL-GBW-33V3.pdf?lipi=urn%3Ali%3Apage%3Ad_flagship3_messag...

HardFault with unsigned short

Posted on November 17, 2017 at 15:03Hi all,I'm working on my program to adapt it with the STM32F072C8, the program works on the LPC1115 and after I've translated for the ST, I found a problem.. I've this array ( unsigned short Example[254] ) but whe...

Resolved! what's wrong with my ADC DMA initialization?

Posted on November 15, 2017 at 22:13 Hello, I'm trying to trigger an ADC conversion externally from TRGO2 and store it to a buffer through DMA. However, it doesn't appear that anything is being written to that buffer. Could someone please look...

G S by Associate II
  • 2682 Views
  • 7 replies
  • 0 kudos

STM32f3 ADC & DMA Problem

Posted on October 04, 2015 at 15:30Hey,i am trying hard to get the DMA & ADC controller to work on my discovery board. I want to sample PA1&2, which are connected to current shunts.the following code is not working, and i am not sure why. the DMA_IT...

Please make HAL examples visible in the net

Posted on November 13, 2017 at 23:54Luckily Google is not looking into our HDs (yet?), so people do not find these at first: C:\Users\XXXX\STM32Cube\Repository\STM32Cube_FW_F7_V1.8.0\Projects\STM32746G-Discovery. And so onSo if you put all examples ...

LMI2 by Lead
  • 715 Views
  • 1 replies
  • 0 kudos

Float Assignment Causing HardFault

Posted on November 09, 2017 at 21:27Hello. I am trying to control a step motor with a driver like m542 stepper driver. I can control the rotation speed and direction of the motor. I'm working with STM32F4-Discovery to get prototype done. Everything ...

How to interface 1Gbit Parallel NOR Flash with STM32F437?

Posted on November 14, 2017 at 10:15 Hi, I have a S29GL01GS 1Gbit parallel NOR flash (26 address lines [A0-A25] & 16 data lines),if i configure the chip select to be used in Bank1 (NE1) ,it has an address range of 0x60000000 to 0x63FFFFFF,which is ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.