2017-11-13 2:54 PM
Luckily Google is not looking into our HDs (yet?), so people do not find these at first: C:\Users\XXXX\STM32Cube\Repository\STM32Cube_FW_F7_V1.8.0\Projects\STM32746G-Discovery. And so on
So if you put all examples as sticky posts in this forum, it would be much easier to tell users how to get ADC interrupts working. And I am sure there are many harder cases like USB and ETHERNET.
2017-11-17 7:11 AM
Hello
Michael.Lei
,I think the best way is to give the user the link to download the package that he needs:
package for example. And then to indicate the name of the example and its path: Example: 'HID_Standalone' found under the path below:
STM32Cube_FW_F4_V1.0\Projects\STM32446E_EVAL\Applications\USB_Device\HID_Standalone
Khouloud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.