STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using the backup SRAM?

Posted on November 30, 2017 at 12:35MCU: STM32F777IIHow can I use the backup SRAM to store non volatile data? Are there any examples?Is there also way to let the compiler know that this is the area of RAM to use for allocating these variable which I...

Resolved! ADC value not correct for ADC_CHANNEL_12

Posted on September 29, 2017 at 14:32Hello,I am using STM32F446 MCU. ADC chnanel 10 & ADC channel 12.ADC ref voltage is 3.0V.I am getting 0 count for 0v on ADC channel 10.But I get ADC count value 87 for ADC channel 12. which calculates to 1 V.what ...

ra.pamod by Associate III
  • 1636 Views
  • 3 replies
  • 0 kudos

Problems with DSP(Fourier transform)

Posted on November 26, 2017 at 06:27 Dear Community, I'm new to programming and STM32 microconrollers, though, I have to perform FFT of 50Hz voltage. Well, after defining my core by ARM_MATH_CM7 in arm_math.h, I get error messages like: ...

stm32 Can Bus receive Error

Posted on February 24, 2015 at 10:50  The original post was too long to process during our migration. Please click on the attachment to read the original post.

CubeMX code generation issue

Posted on September 28, 2017 at 10:00Using CubeMX with CubeL4 1.9.0, I have the following problem.I'm using FreeRTOS with tasks defined as either weak, or external (weak is only used because the default task cannot be external for whatever reason). ...

HAL RTC BUG

Posted on September 02, 2014 at 10:40There appears to be a bug in the HAL drivers for the RTC. I have only recently migrated to STM micros and am in the process of rewriting a number of projects to use them.  I have a project running on a STM32F405R...

malcolm2 by Associate II
  • 2911 Views
  • 4 replies
  • 0 kudos

X-CUBE-SOUNDTER1: how to set I2S clock?

Posted on November 29, 2017 at 22:47Hi, I have a nucleo f401re board and a x-nucleo-cca01m1 shield mounting STA350BW IC. Nucleo transmits data as a master to the shield using I2S half duplex communication. I want to know what is Master Clock's purpo...

M7 and H7 cache (sharable performance)

Posted on November 27, 2017 at 11:15Dear All,I have some questions concerning the cache of the cortex M7 & H7 micro controller.I use an external SDRAM and the data and instruction caches are activated. Now, if I define the region as 'shareable', I l...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.