2017-09-28 1:00 AM
Using CubeMX with CubeL4 1.9.0, I have the following problem.
I'm using FreeRTOS with tasks defined as either weak, or external (weak is only used because the default task cannot be external for whatever reason). My weak ApplicationTask is generated as follows:
/* ApplicationTask function */
__weak void ApplicationTask(void const * argument)
{ /* init code for USB_DEVICE */ MX_USB_DEVICE_Init(); /* USER CODE BEGIN ApplicationTask */ /* Infinite loop */ for(;;) { osDelay(1); } /* USER CODE END ApplicationTask */}/* USER CODE BEGIN Application */ /* Infinite loop */ for(;;) { osDelay(1); }/* USER CODE END Application */Notice the user code segment named Application after the actual function. This causes the generated code to not compile without deleting this 'surplus' block.
2017-10-19 2:39 AM
Dear user,
This issue will be fixed in our next release 4.23.
Best regards.
2017-11-30 1:10 AM
Hello,
Just for reference, this issue was NOT fixed in 4.23.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.