STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L432KC - Timer DMA Triggering ADC DMA?

Posted on February 17, 2017 at 05:19 Hi, On my larger project, I would like to be able to generate a timer that will trigger an ADC read on each rising edge. I was able to tackle this problem by creating a smaller project and executing it! Sup...

Nolan L by Associate III
  • 7262 Views
  • 7 replies
  • 0 kudos

Where is STM32 RTC counter value? (Not F1 family)

Posted on December 08, 2016 at 20:29Hi,In the scheduling system we use we need a simple 32kHz low power counter value. Exactly like in the stm32F1 family is present.But in any other family, the RTC registers are replaced by Time and Date registers.I...

Resolved! STM32l4 in stop2 mode with rtc alarm

Posted on December 21, 2017 at 07:47Dear all i want to wakeup stm32l4 in every two minute from stop2 mode using RTC,give me suggestion.I am using example code from st and trying  PWR_STOP2_RTC on my custom board,i am finding that l4 is not going in ...

Receive UART WWDG_IRQHandler infinite loop

Posted on December 21, 2017 at 14:25Good morning. I'v tried to perform an UART receive on stm32f407vg board using RXNE interrupt. But when i execute the code it is blocked on WWDG_IRQHandler infinite loop. I post my code:#include 'stm32f4xx.h'#inclu...

Resolved! Toggling GPIO STM32F407VGT6

Posted on December 19, 2017 at 05:50Hello,I am using the Mikro Pro C IDE to write a simple program to toggle GPIOA pin 0 on a STM32F407VGT6. When I compile I get several errors, but I don't think it has to do with an error in my code, more or less a...

0690X00000609FsQAI.png

how would i change this code to it four bit rather than 8?

Posted on December 20, 2017 at 14:02#ifndef _LCD_H_ #define _LCD_H_ #define LCD_PORT GPIOD #define LCD_RS_pin 11 #define LCD_RW_pin 12 #define LCD_E_pin 13 #define LCD_D0_pin 0 #define LCD_LINE1 0x80 #define LCD_LINE2 0xc0 #define set_LCD_RS() LCD_P...

j g by Associate II
  • 1108 Views
  • 1 replies
  • 0 kudos

programming STM32F0 controller rs485 half duplex mode

Posted on December 21, 2017 at 12:46Hello,We are using STM32F030 in our project. We are using RS485 half duplex communication for interaction with other boards in our system. Using the same half duplex communication channel, we would like to update ...

ravi b by Associate
  • 810 Views
  • 0 replies
  • 0 kudos

How to detect end of SPI transmission?

Posted on December 20, 2017 at 13:27STM32F030.I am transmitting multiple words via spi to some shift registers and need to latch the shift registers when the transmission of the last word is finished. The latch signal is GPIO. Device is master.I don...

toby2 by Senior
  • 6413 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.