STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TRF7960 STM32F407 SPI communication issue

Posted on December 14, 2017 at 04:10Hi -We are trying to integration TRF7960 with our custom hardware which has STM32F407 processor (via SPI). As per errata 1.1 on TRF7960, we need to switch the polarity of clock during write & read operation (Errat...

pramuka by Associate II
  • 1575 Views
  • 2 replies
  • 0 kudos

how would i turn this from 8 bit to 4 bit??

Posted on December 22, 2017 at 16:13&sharpinclude 'lcd.h'void lcd_delayus(unsigned int us) //blocking delay for LCD, argument is approximate number of micro-seconds to delay{ unsigned char i; while(us--) { for(i=0; i<SystemCoreClock/4000000; i++); }...

j g by Associate II
  • 1051 Views
  • 1 replies
  • 0 kudos

LWIP ....what am i doing wrong?

Posted on December 21, 2017 at 22:38I am trying to get LWIP and use it as a client... I scoured demos and I was able to produce what I think is working code. I set it up so I simply spam the server with a message so i can see that i am actually send...

Andrew C by Associate III
  • 1022 Views
  • 2 replies
  • 0 kudos

Resolved! Power-up problem STM32L4

Posted on December 21, 2017 at 13:38Hello,Having a problem to startup the STM32L4 MCU. After powering the board it seems like the controller does not start or get stuck. Running with a debugger works fine but when removing the debugger connection an...

Resolved! External MCU programming STM32

Posted on December 21, 2017 at 13:25I've an Nucleo-f091rc, and i need using this board to programming an external STM32F070, using SWDIO, I've connected SWDIO, SWDCLK, NRST and GND. My external MCU have external 3.3V. When I try to connect I receive...

STM32L4 and F1 RTC Alarm HAL libraries

Posted on December 22, 2017 at 12:26Hi,HAL libraries are used to make easy project porting from a series or MCU to another one ...I just found a trouble, i used RTC ALARM in L4 and L0 MCU and set a fixed time to make alarm each 24 hours. it works wi...

mbedTLS Client ssl handshake failed

Posted on December 22, 2017 at 11:45I am using STM32F769I-DISCO. and using STM32Cube_FW_F7_V1.8.0I want to test mbedTLS SSL_Client example.I am using STM32Cube_FW_F7_V1.8.0\Utilities\PC_Software\ssl_server\ssl_server.exe as SSL server in Windows 7.W...

ritesh by Associate II
  • 1734 Views
  • 0 replies
  • 0 kudos

Problem with Flash loader demonstrator on STM32L452RE

Posted on October 18, 2017 at 14:35Hello,I'm trying to use the flash loader demonstartor change the software on my STM32L452RE.I place my device in bootloader mode, and I manage to connect using Flash Loader demonstrator, but then I'm on a page aski...

Resolved! CubeMX generator have a problems

Posted on December 20, 2017 at 18:21Hello guys! Help me please... I have problems with the CubeMX, can not generator code create project((( Operating system Linux Mint 18

Hosting by Associate III
  • 2061 Views
  • 4 replies
  • 0 kudos

STM32L4R9-EVAL UART Promblem

Posted on December 19, 2017 at 12:48Hello, I'm struggling to make (any of) the UART examples for the STM32L4R9-EVAL board work, so far without any success. Has any one here was able to get any data from the UART port (through the ST_Link interface) ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.