STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LD1 on the ST-Link board stays red?

Posted on December 20, 2017 at 11:17Hey guys, I'm trying to do something that might be really a noobish thing (will ask in a different thread, and I recognize that there's a strange thing happening. I'm using an STM32 Nucleo64 L073RZI am trying to s...

ST-Link/V2 error

Posted on December 21, 2017 at 08:39I have some problems connecting ST-link/V2 to STM32L0x1 device, especially with OpenOCDST-Link_cli.exe connects but log-file shows errors:Error (0x10) after target cmd F2 30 A3 00 00 00 00 00 00 00Error (19) while...

Hi, Facing USB Write issue when USB traffic is more.

Posted on May 03, 2017 at 16:29Hi,We are using STM32F072C8 device and we are using USB CDC Interface when communicating with PC.When USB bus traffic is low everything is working fine.But when USB bus traffic is heavy we observed during USB CDC Write...

Looking for fast startup STM32

Posted on December 21, 2017 at 03:52We have a project that using a wiegand sensor to power the mcu and update the counter to FRAM through SPI. there will be a 10us width regulated power supply from wiegand, all the process need to be done in 10us wi...

construction error with qt creator stm32l152re

Posted on December 20, 2017 at 23:43 I'm new to microcontroller programming and I have a question. I'm trying to set up a stm32l152re card in the qtcreator and the same error appears at the time of compiling the project shrink arm-none-eabi-gc...

Resolved! STM32F0 series. Waiting for Page Write/Erase completion.

Posted on December 20, 2017 at 18:20Hello all.HAL uses function 'FLASH_WaitForLastOperation' for polling flash 'BUSY' flag, while performing flash page erase or flash write. How can this function be executed from flash if flash bus is blocked during...

baranovus by Associate III
  • 1456 Views
  • 3 replies
  • 0 kudos

Which STM32 MCU has the fastest ADC?

Posted on December 20, 2017 at 15:51I know of the STM32F303 line with 5MS/s (0.2us),the F378 with slower ADCs but 16-bitand some F4/F7 devices with also slower than the F303 ADCs.But which STM32 has the fastest ADC regarding the complete conversion ...

how would i turn this into 4 bit mode?

Posted on December 20, 2017 at 14:06[code]#include 'lcd.h' void lcd_delayus(unsigned int us) //blocking delay for LCD, argument is approximate number of micro-seconds to delay { unsigned char i; while(us--) { for(i=0; iBSRR=(0xff<<(LCD_D0_pin+16)); ...

j g by Associate II
  • 774 Views
  • 0 replies
  • 0 kudos

sd-card fr_disk_err

Posted on December 18, 2017 at 14:20hi....cubemx ver 4.22.1 is compatible with firmware package 1.16.0 .....even though it is not working properly for sd-card operations.   i have executed open/read/write operations correctly first but then again ge...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.